cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 high cycle flash read.

MVanb.1
Associate II

What is the correct way to read high cycle flash data.
When i read address 0x916800 i get a Hard fault. Clearing and writing the this address works fine.
With reading i have a problem. bank 2 has EDATA enabled for the last 2 pages.

Can you give me a code example for reading the memory correctly?

4 REPLIES 4
Billy OWEN
ST Employee

Hi @MVanb.1 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

Hi,

Could you please share the method to read data from the high-cycle flash ?
Regards

Greg

mahirmahota
Associate III

Hi! Did you end up getting a solution for this? I'm also trying to get high cycle flash up and running for an H5

STOne-32
ST Employee

Dear @mahirmahota ,

You can look to our example here :

STM32CubeH5/Projects/NUCLEO-H563ZI/Examples/FLASH/FLASH_EDATA_EraseProgram/Src/main.c at main · STMicroelectronics/STM32CubeH5 · GitHub

You need to configure the MPU region with right address of EDATA 

 

/* MPU Configuration--------------------------------------------------------*/
/* By default, all the AHB memory range is cacheable. For regions where caching is not
practical (High-cycle data area), MPU has to be used to disable local cacheability.
*/

like this :

static void MPU_Config(void)
{
MPU_Attributes_InitTypeDef attr;
MPU_Region_InitTypeDef region;

/* Disable MPU before perloading and config update */
HAL_MPU_Disable();

/* Define cacheable memory via MPU */
attr.Number = MPU_ATTRIBUTES_NUMBER0;
attr.Attributes = 0 ;
HAL_MPU_ConfigMemoryAttributes(&attr);

/* BaseAddress-LimitAddress configuration */
region.Enable = MPU_REGION_ENABLE;
region.Number = MPU_REGION_NUMBER0;
region.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
region.BaseAddress = EDATA_USER_START_ADDR;
region.LimitAddress = EDATA_USER_END_ADDR;
region.AccessPermission = MPU_REGION_ALL_RW;
region.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
region.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
HAL_MPU_ConfigRegion(&region);

/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}

Also, have a look on our Reference Manual on the way, we read these Areas : OTP, RO and High Cycle Data - EDATA.

 

STOne32_0-1747076864777.png

Hope it is helping.

STOne-32.