cancel
Showing results for 
Search instead for 
Did you mean: 

stm32g491cet6 ADC and Hal_Delay not working

vsilv.1
Associate II

Hello!

I have a number of issues with stm32g491cet6.

When using the ADC interrupt, it remains in an infinite loop. When using the HAL_Delay () function, an infinite loop also results.

The code is simple and runs on the application board with stm32f103 but not on stm32g491cet6 (two separate projects of course).

The PWM work good.

Below is the code from stm32g491cet6.

0 REPLIES 0