2023-12-17 10:41 PM
I have a project , used regular conversion ADC1 Vrefint Channel and Temperature Channel, and used injected conversion ADC2 extern Channel(ext.CH1 and CH2).
ADC2 CH2 connect 2000mV voltage , CH1 is changed. If CH1 over 3.6V,the CH2 conversion is error.I tryed more channel , it all error.But in my function , I should not control this voltage to below 3.3V or 3.6V.
Solved! Go to Solution.
2023-12-18 05:51 AM
ADC inputs should be limited to 0-VREF+ per the datasheet. Values outside of this range can damage the chip and lead to undesirable behavior.
If you have a signal higher than that, use a voltage divider or an op-amp divider to get it into the correct range.
2023-12-18 05:51 AM
ADC inputs should be limited to 0-VREF+ per the datasheet. Values outside of this range can damage the chip and lead to undesirable behavior.
If you have a signal higher than that, use a voltage divider or an op-amp divider to get it into the correct range.