cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32G431KBU6 CANFD can't work when BRS On?

eason_Yi
Associate II

Hi community:

     I'm using CANFD on stm32g431kbu6 board, but I find some issue that CANFD cant work normally with BRS ON,my config of CANFD show in the comments。Does anyone know about this?

 

Thanks

12 REPLIES 12

You need to increase TSEG1 and TSEG2 as much as possible an decrease the prescaler either for Nominal or data phases.

TSEG1 ~= 80% (TSEG1+TSEG2) for sampling point at 80%

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Because my slave CANFD device is working in sampling point at 75% of data phase, data baud is 5MHz, so I want to set at 75%, it seems work good now, I'll conduct  pressure testing for a period of time.If this kind issues happen again, I'll try your advice.

Thanks

75% or 80% doesn't make much difference.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.