cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32h755: hardware questions

baselimadt
Associate III

Hi 

I am developing a board with two MCU on it (stm32h755), and I am going to programme these two controllers from the same connector using only two lines (SWDIO SWCLK), I have connected same CLOCK line to both MCUs directly, and the SWDIO to a switch to select which MCU to programme, is this connection fine??
Also this MCU has the CANFD, but I want to use normal CAN, is it fine to connect it to a normal CAN transceiver not CANFD one??.
thanks

baselimadt_0-1733228227067.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

SWCLK is an input to the MCU so you can share it with both MCUs: https://developer.arm.com/documentation/100893/1-0/Debug-and-trace-interface/Serial-Wire-Debug-signals

SofLit_0-1733242493678.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

To program more than one MCU you need a daisy chain configuration where serial debug does not support this feature according to this post. You can do it with JTAG, see this post.

For your last question, I didn't understand well your question. If you mean that you need to use a CAN transceiver 2.0A/2.0B transceiver with FDCAN interface, yes but you can't exceed 1Mb/s.

See this FAQ: https://community.st.com/t5/stm32-mcus/faq-can-i-use-a-can2-0a-can2-0b-transceiver-to-transmit-canfd/ta-p/689733

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi Soflit.
to make it clear on the first question, I want to prgramme each MCU alone using STlinkv2, but both MCUs are sharing the clock line only and the data line is go to a switch to determine wich MCU to be connected with the STlinkv2.

and thanks you answered the second question I don't want to exceed 1Mb/s

SWCLK is an input to the MCU so you can share it with both MCUs: https://developer.arm.com/documentation/100893/1-0/Debug-and-trace-interface/Serial-Wire-Debug-signals

SofLit_0-1733242493678.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.