2019-10-15 05:31 AM
The manual writes: At startup, a BOOT0 pin (or nBOOT0 option bit) and an nBOOT1 option bit are used to select one of three boot options:
But I did not find nBOOT1 in Pin definition. I don't know how to configure the pins of BOOT mode.
2019-10-15 05:57 AM
Hi,
nBOOT1 is not a pin, it is only an option bit that has to be programmed either by the debugger or by your program.