cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G431KB BOOT MODE

km naxin
Associate II

The manual writes: At startup, a BOOT0 pin (or nBOOT0 option bit) and an nBOOT1 option bit are used to select one of three boot options:

But I did not find nBOOT1 in Pin definition. I don't know how to configure the pins of BOOT mode.

1 REPLY 1
Kraal
Senior III

Hi,

nBOOT1 is not a pin, it is only an option bit that has to be programmed either by the debugger or by your program.