2020-04-13 7:21 PM
Hi,
The documentation between the STM32G4 RM0440 Rev 3 and between the individual MCU specifications is inconsistent when it comes to the PLL limits. In the documentation for RCC_PLLCFGR we have the following two statements:
PLLN: "The software has to set correctly these bits to assure that the VCO output frequency is between 64 and 344 MHz."
PLLM: "The software has to set these bits correctly to ensure that the VCO input frequency ranges from 2.66 MHz to 8 MHz."
However, in DS12288 Rev 2 (data sheet for STM32G474xB xC and xE), under "5.3.9 PLL Characteristics", we have the following limits:
fVCO_OUT: 96 MHz to 344 MHz (Range 1) or 96 MHz to 128 MHz (Range 2)
fPLL_IN: 2.66 MHz to 16 MHz
Could we get clarification on what the correct limits are?
Thanks!
2020-04-14 6:14 AM
Hello @Terry Greeniaus ,
Thank you for highlighting this.
The correct values of "PLL Characteristics" are in the datasheets.
We will modify RM0440 and remove wrong statements (there should be no numeric values – just reference to datasheet).
Best Regards,
Imen