cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 chaos in internal ref

MM..1
Chief III

Hi, i start design on G4 and am confused with internal ref in MX.

1. Internal REF for ADC isnt real internal, but Vref

2.Internal ref for comparators is 1/2 1/4 3/4 ... , but from what ?

3. ADC stop working without VREF+ pin voltage, but comparator works

4. ADC start working enable out internal ref to VREF buff 

5. internal ref can be selected to one from 3 voltages , but after select is global for ??periph ?

 

Can some ST make info short and clean on this pls.

0 REPLIES 0