2021-11-22 12:08 AM
My target device is a STM32G0B1VE which has PE but according to RM0444 Reference manual for STM32G0x1 chips the description of EXTI_EXTICRx register says that combination for PE is not present (reserved). Is it really no possible to use PE for an external interrupt? I don't have hardware yet so I cannot test it.
Solved! Go to Solution.
2021-11-24 7:19 AM
Hello @JOtru.1 and welcome to the Community :)
I confirm that Port E is set to enter the EXTI, and the RM should be fixed.
Thank you for your contribution and spotting this out.
I closed this thread by marking "Select as Best", as this will help other users find that answer faster.
Imen
2021-11-22 7:29 AM
Probably the RM was written when there weren't any chips with a GPIOE and wasn't fully updated. I would be surprised if it didn't work. I don't have a chip to test.
2021-11-22 10:12 PM
I have the same opinion, STM32G0B1 and STM32G0C1 are the latest devices from the line. Also older IDEs doesn't support them so I suppose the RM is probably outdated in this way.
2021-11-24 7:19 AM
Hello @JOtru.1 and welcome to the Community :)
I confirm that Port E is set to enter the EXTI, and the RM should be fixed.
Thank you for your contribution and spotting this out.
I closed this thread by marking "Select as Best", as this will help other users find that answer faster.
Imen