cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0x1 external interrupt from PE possible?

JOtru.1
Associate

My target device is a STM32G0B1VE which has PE but according to RM0444 Reference manual for STM32G0x1 chips the description of EXTI_EXTICRx register says that combination for PE is not present (reserved). Is it really no possible to use PE for an external interrupt? I don't have hardware yet so I cannot test it.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @JOtru.1​ and welcome to the Community :)

I confirm that Port E is set to enter the EXTI, and the RM should be fixed.

Thank you for your contribution and spotting this out.

I closed this thread by marking "Select as Best", as this will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
TDK
Super User

Probably the RM was written when there weren't any chips with a GPIOE and wasn't fully updated. I would be surprised if it didn't work. I don't have a chip to test.

0693W00000GYSlMQAX.png

If you feel a post has answered your question, please click "Accept as Solution".
JOtru.1
Associate

I have the same opinion, STM32G0B1 and STM32G0C1 are the latest devices from the line. Also older IDEs doesn't support them so I suppose the RM is probably outdated in this way.

Imen.D
ST Employee

Hello @JOtru.1​ and welcome to the Community :)

I confirm that Port E is set to enter the EXTI, and the RM should be fixed.

Thank you for your contribution and spotting this out.

I closed this thread by marking "Select as Best", as this will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen