2023-07-15 2:13 PM
Hi everyone,
I am not sure what is the difference between GP and N version of the chip. What I can find in the datasheet is that N version has additional VDDIO2 and VSS pins. If that is the only difference, what changes do these pins bring?
Thanks!
Solved! Go to Solution.
2023-07-16 12:41 AM
This is intended for USB/USBCPD applications where the USB side runs at different voltage than the rest of processor/interfaces.
Note, that in the both 32-pin packages the difference is more dramatic than just presence of VDDIO2 (and related absence of PC6/7) - this is in line with the same "GP"/"N" variant in 'G07x https://community.st.com/t5/stm32-mcu-products/difference-between-quot-gp-version-quot-vs-quot-pd-version-quot/td-p/183326
Note, that nature of VDDIO2 "ring" (IO supply domain) in 'G0 is not the same as VDDIO2/VDDUSB in some other STM32, as there is no isolation switch.
Also, RM0444 says, " Although VDDIO2 isindependent of VDD or VDDA , it must not be applied without valid VDD"; however, I can find no mention of this constraint in the 'G0B1 datasheet... ( @Imen.D , can this detail please be clarified? Thanks.)
JW
2023-07-16 12:41 AM
This is intended for USB/USBCPD applications where the USB side runs at different voltage than the rest of processor/interfaces.
Note, that in the both 32-pin packages the difference is more dramatic than just presence of VDDIO2 (and related absence of PC6/7) - this is in line with the same "GP"/"N" variant in 'G07x https://community.st.com/t5/stm32-mcu-products/difference-between-quot-gp-version-quot-vs-quot-pd-version-quot/td-p/183326
Note, that nature of VDDIO2 "ring" (IO supply domain) in 'G0 is not the same as VDDIO2/VDDUSB in some other STM32, as there is no isolation switch.
Also, RM0444 says, " Although VDDIO2 isindependent of VDD or VDDA , it must not be applied without valid VDD"; however, I can find no mention of this constraint in the 'G0B1 datasheet... ( @Imen.D , can this detail please be clarified? Thanks.)
JW
2023-07-17 5:02 AM
Thanks for your reply. Based on your answer, I searched a bit more and found this:
It seems that it is not only for USB, but also for different peripherals. It is convenient for environments with different bus voltages. In my case (LQFP-48), I have main voltage level of 3.3V. I can now set VDDIO2 to 1.8V and work directly with the modem without using a level shifter.