cancel
Showing results for 
Search instead for 
Did you mean: 

stm32g071rbIx or stm32g071rbTx?

Singh12
Associate

I am using Keil Development environment for stm32g071 nucleo board. Which device should I choose? stm32g071rbIx or stm32g071rbTx? 

And how do I decide which one is correct for me?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @Singh12​, to the community!

It depends on your requirements which device to be used (see datasheet:(

  • STM32G071RBIx: "I" stands for UFBGA package
  • STM32G071RBTx: "T" stands for LQFP package

The NUCLEO-G071RB uses the STM32G071RBT6.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @Singh12​, to the community!

It depends on your requirements which device to be used (see datasheet:(

  • STM32G071RBIx: "I" stands for UFBGA package
  • STM32G071RBTx: "T" stands for LQFP package

The NUCLEO-G071RB uses the STM32G071RBT6.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.