2021-05-17 7:25 AM
Hello!
I have ported overt X-CUBE-CLKTRIM to the STM32L4R5ZI Nucleo board. Unfortunately the callback HAL_TIM_IC_CaptureCallback is not called. Which results in the HSI and MSI frequency measurements to be calculated as 0.
I have put a function generator to act as the HSI (X3) and I have converted the project for the nucleo board via the Target setting found in the project properties.
2021-05-17 7:30 AM
I've also added a function generator to act as the HSI at 8MHz.
2021-05-18 12:50 AM
So it looks as though the timer15 does not fire and is used to measure the HSI and MSI frequencies. However, Timer16 which is used for LSI does work.