cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G030J6M6, SPI

STere.1719
Associate II

Hello.

Is it possible to use hardware SPI with  STM32G030J6M6 (SO-8)?

SPI1 use PA1 (NRST pin) for CLK without remap possibility.

SPI2 also use PA1 (NRST pin) for CLK, but has CLK remap to PC14. In that case no MOSI pin.

I try to use SPI1. PA1 configured as AF0 PP.

Writing to the SPI1->DR register results in a reboot.

0 REPLIES 0