cancel
Showing results for 
Search instead for 
Did you mean: 

What are the STM32G030J6M6 pin functions after reset

gerhard
Associate II

The STM32G030J6M6 is the SO8N device.

The Datasheet lists different functions upon reset for pins 4, 5, 8

Any help appreciated

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

The SWD pins (PA13/PA14) are initialized as such at reset. Others are initialized in high impedance input mode.

NRST is NRST, unless disabled in option bytes.

> The Datasheet lists different functions upon reset for pins 4, 5, 8

Where? I only see it call out PA13/PA14 (pins 7 and 8).

If you feel a post has answered your question, please click "Accept as Solution".