2024-09-21 5:42 AM - last edited on 2024-09-21 6:21 AM by Peter BENSCH
Have an issue with connection I2C sensor to STM32G030 chip.
Function HAL_I2C_IsDeviceReady alvais return HAL_ERROR.
Looks like this controller are not support I2C master, but documentation said:
Features of the I2C peripheral:
I2C-bus specification and user manual rev. 5 compatibility:
Slave and master modes, multimaster capability
Solved! Go to Solution.
2024-09-21 6:41 AM
Yes, of course it does I2C master.
HAL_I2C_IsDeviceReady returns HAL_ERROR if your device does not respond. Perhaps you are not using the correct slave address, or the slave is not powered or otherwise hooked up right. Slave addresses should be left-shifted by one bit.
2024-09-21 6:41 AM
Yes, of course it does I2C master.
HAL_I2C_IsDeviceReady returns HAL_ERROR if your device does not respond. Perhaps you are not using the correct slave address, or the slave is not powered or otherwise hooked up right. Slave addresses should be left-shifted by one bit.
2024-09-21 10:11 AM
It's looks strange because I checked on STM32F401 and there works fine, sensor detected. So, I know exactly the i2c sensor address and wires connected correct. Also checked signals SDA and SCL using oscilloscope, they show nothing. Looks like I2C are not started or it in slave mode and waiting for master start communication
2024-09-21 10:48 AM
Add configuration screen of STM32G030.
Have a two boards with this chip and for both I2c are not worked.
Also add config of STM32F401. Where i2c works. There MASTER section present. In STM32G030 no MASTER section.
2024-09-21 5:20 PM
The peripheral is different and so the configuration screen is different. But it can be an I2C master. Perhaps share your code. What does HAL_I2C_IsDeviceReady return?
2024-09-22 1:04 AM
Found the issue. First one SDA pin was interrupted by jumper. Main purpose of this pin use for external oscillator, Second one, device address specified by manufacture need shift to one bit (((.