2015-07-27 2:25 AM
2015-07-27 9:13 AM
Hi karpavicius.linas,
Have a look at the example under STM32Cube_FW_F7_V1.1.0\Projects\STM32746G-Discovery\Examples\SPI, maybe it can help you even if it is in normal mode. -Shahrzed-2015-07-27 8:44 PM
No, it must be in Circular mode. I usually start by looking to examples, and SPI example does not support circular mode by the looks of it
It is starting to work for me, MOSI line is active, but enabling SPI in circular mode only works second time, that means, first debugging session it works, second it does not, third it works, fourth it does not. So, i have no idea what going on.2015-07-28 11:58 PM
this is code i am running. As i said, it work at odd times (1,3,5,7 debugging season at same power up, but not at second, fourth, six debugging season)
extern uint8_t DataRx[];
extern uint8_t DataTx[];
SPI_HandleTypeDef hspi2;
void SPI_Config(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOC_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
__SPI2_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLED;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;
hspi2.Init.CRCPolynomial = 10;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLED;
HAL_SPI_Init(&hspi2);
__HAL_RCC_DMA1_CLK_ENABLE();
DMA_HandleTypeDef hdma_spi2_rx;
DMA_HandleTypeDef hdma_spi2_tx;
//HAL_DMA_DeInit(&hdma_spi2_rx);
//HAL_DMA_DeInit(&hdma_spi2_tx);
hdma_spi2_rx.Instance = DMA1_Stream3;
hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_rx.Init.Mode = DMA_CIRCULAR;
hdma_spi2_rx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi2_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi2_rx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi2_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_spi2_rx);
HAL_DMA_Start(&hdma_spi2_rx,(uint32_t)(&(SPI2->DR)),(uint32_t)(&DataRx), 5000);
//__HAL_LINKDMA(hspi,hdmarx,hdma_spi5_rx);
hdma_spi2_tx.Instance = DMA1_Stream4;
hdma_spi2_tx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_tx.Init.Mode = DMA_CIRCULAR;
hdma_spi2_tx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi2_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi2_tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi2_tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_spi2_tx);
HAL_DMA_Start(&hdma_spi2_tx, (uint32_t)&DataTx, (uint32_t)(&SPI2->DR),5000);
//__HAL_LINKDMA(hspi,hdmatx,hdma_spi5_tx);
HAL_NVIC_SetPriority(DMA2_Stream3_IRQn,0,0);
HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);
HAL_NVIC_SetPriority(DMA2_Stream4_IRQn,0,0);
HAL_NVIC_EnableIRQ(DMA2_Stream4_IRQn);
SPI2->CR2 |= 0x0002;
SPI2->CR2 |= 0x0001;
SPI2->CR1 |= SPI_CR1_SPE;
}
2015-07-30 2:08 AM
SPI_HandleTypeDef hspi2;
void SPI_Config(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOC_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
__SPI2_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLED;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLED;
HAL_SPI_Init(&hspi2);
__HAL_RCC_DMA1_CLK_ENABLE();
DMA_HandleTypeDef hdma_spi2_rx;
DMA_HandleTypeDef hdma_spi2_tx;
DMA1_Stream3->CR &= ~((uint32_t)DMA_SxCR_EN);
DMA1_Stream3->CR = 0;
DMA1_Stream3->NDTR = 0;
DMA1_Stream3->PAR = 0;
DMA1_Stream3->M0AR = 0;
DMA1_Stream3->M1AR = 0;
DMA1_Stream3->FCR = (uint32_t)0x00000021;
DMA1->LIFCR = DMA_Stream3_IT_MASK;
DMA1_Stream4->CR &= ~((uint32_t)DMA_SxCR_EN);
DMA1_Stream4->CR = 0;
DMA1_Stream4->NDTR = 0;
DMA1_Stream4->PAR = 0;
DMA1_Stream4->M0AR = 0;
DMA1_Stream4->M1AR = 0;
DMA1_Stream4->FCR = (uint32_t)0x00000021;
DMA1->LIFCR = DMA_Stream4_IT_MASK;
hdma_spi2_rx.Instance = DMA1_Stream3;
hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_rx.Init.Mode = DMA_CIRCULAR;
hdma_spi2_rx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi2_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi2_rx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi2_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_spi2_rx);
HAL_DMA_Start(&hdma_spi2_rx,(uint32_t)(&(SPI2->DR)),(uint32_t)(&DataRx), BUFFERSIZE);
//__HAL_LINKDMA(hspi,hdmarx,hdma_spi5_rx);
hdma_spi2_tx.Instance = DMA1_Stream4;
hdma_spi2_tx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_tx.Init.Mode = DMA_CIRCULAR;
hdma_spi2_tx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi2_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi2_tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi2_tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_spi2_tx);
HAL_DMA_Start(&hdma_spi2_tx, (uint32_t)&DataTx, (uint32_t)(&SPI2->DR),BUFFERSIZE);
HAL_NVIC_SetPriority(DMA2_Stream3_IRQn,0,0);
HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);
HAL_NVIC_SetPriority(DMA2_Stream4_IRQn,0,0);
HAL_NVIC_EnableIRQ(DMA2_Stream4_IRQn);
SPI2->CR2 |= 0x0002;
SPI2->CR2 |= 0x0001;
SPI2->CR1 |= SPI_CR1_SPE;
}
This is my setup i am using right now. Newer get correct values, and sometimes it just don't work. So, any one can help me out ?
Also, what is __HAL_LINKDMA(); and do i need one ?
2015-07-30 4:13 AM
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00189702.pdf
(Description of STM32F7xx HAL drivers) to understand the purpose of HAL functions & macros and to know how structures of peripherals are defined.So, for example, __HAL_LINKDMA is the macro that MUST be used in order to associate the initialized DMA handle to the SPI DMA handle (don't understand why you commented it).In the UM1905, there is a chapter dedicated for HAL SPI driver.You find there the following recommendations if you need to use DMA process:To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-08-04 2:55 AM
So two weeks are in, and this problem still remains. ( i did try to read programming manual as well as HAL programming reference )
I don't exactly understand why I needvoid SPIx_DMA_RX_IRQHandler(void)
{
HAL_DMA_IRQHandler(hspi2.hdmarx);
}
void SPIx_DMA_TX_IRQHandler(void)
{
HAL_DMA_IRQHandler(hspi2.hdmatx);
}
if it's in circular mode, i don't have to deal with any SPI and DMA related stuff, after i initialize it. I don't use transmit complete interrupts or any thing that can cause processor to execute some code.
And to save time i always start with examples, don't say lookup examples or programming references, because i did all this to best of my ability ( if i have any)
extern uint8_t DataRx[];
extern uint8_t DataTx[];
DMA_HandleTypeDef hdma_spi2_rx;
DMA_HandleTypeDef hdma_spi2_tx;
SPI_HandleTypeDef hspi2;
void SPI_Config(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOC_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
__SPI2_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLED;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLED;
HAL_SPI_Init(&hspi2);
__HAL_RCC_DMA1_CLK_ENABLE();
HAL_DMA_DeInit(&hdma_spi2_tx);
HAL_DMA_DeInit(&hdma_spi2_rx);
HAL_NVIC_DisableIRQ(DMA1_Stream3_IRQn);
HAL_NVIC_DisableIRQ(DMA1_Stream4_IRQn);
hdma_spi2_rx.Instance = DMA1_Stream3;
hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_rx.Init.Mode = DMA_CIRCULAR;
hdma_spi2_rx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi2_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi2_rx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi2_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_spi2_rx);
__HAL_LINKDMA(&hspi2,hdmarx,hdma_spi2_rx);
hdma_spi2_tx.Instance = DMA1_Stream4;
hdma_spi2_tx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_tx.Init.Mode = DMA_CIRCULAR;
hdma_spi2_tx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi2_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi2_tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi2_tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_spi2_tx);
__HAL_LINKDMA(&hspi2,hdmatx,hdma_spi2_tx);
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn,1,1);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
HAL_NVIC_SetPriority(DMA1_Stream4_IRQn,1,0);
HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);
HAL_DMA_Start(&hdma_spi2_rx,(uint32_t)(&(SPI2->DR)),(uint32_t)(&DataRx), BUFFERSIZE);
HAL_DMA_Start(&hdma_spi2_tx,(uint32_t)&DataTx, (uint32_t)(&SPI2->DR),BUFFERSIZE);
SPI2->CR2 |= 0x0002;
SPI2->CR2 |= 0x0001;
SPI2->CR1 |= SPI_CR1_SPE;
}
uint32_t spi_i = 0;
void SPIx_DMA_RX_IRQHandler(void)
{
HAL_DMA_IRQHandler(hspi2.hdmarx);
}
void SPIx_DMA_TX_IRQHandler(void)
{
HAL_DMA_IRQHandler(hspi2.hdmatx);
}
So far i get 0 help with problems, mainly because only people who helped me here works only with SPL.
I don't expect to get answers all the time, but neither only to get, read manual, lookup examples....
And i still need to make DCMI work, i just wonder how much problems i will get with last peace of the puzzle, at least example with be a bit easier to work with ( i hope )