cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L051R + GLASS LCD low power scheme

eduardobernardi7
Associate II
Posted on August 03, 2015 at 20:20

Hello !

We are working in a project that needs a glass lcd display, the average consumption  of the system (MCU + LCD) must be around 50 uA. I always used a msp430 with integrated lcd controller to handle this kind of problems. But now I am very tempted to use a STM32L051R mainly due to the costs and performance.

Anyone here already tried this?

I read the AN2656 and noticed that is possible to interface a glass lcd with the stm32. But the average consumption in this application note was too high.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
stm322399
Senior
Posted on August 03, 2015 at 20:48

Save time and money, using the more expensive STM32L053R.

That MCU has builtin LCD driver .

I used the LCD driver of STM32L152 (the discovery board) and reached a mean current draw of 6µA. This solution has less software, which means less current, and less bugs ! Certainly the fastest way to build whatever you are building.

eduardobernardi7
Associate II
Posted on August 04, 2015 at 12:58

Oh ! Thank you ! , didnt know that st had a stm32 with integrated lcd controller.