cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769I-DISCO Using CAN interface over Arduino connector

BViet.1
Associate III

Hi,

I have a problem with CAN peripheral on this board. I tried the CAN Networking Example from the EVAL board and changed the pin configuration to fit to the Arduino connector.

I found some possible pin configurations:

CAN1_RX on PA11 -> D10

CAN1_TX on PA12 -> D13

CAN1_RX on PB8 -> D15

CAN1_TX on PB9 -> D14

I added an external transceiver from Waveshare (https://www.waveshare.net/w/upload/8/82/SN65HVD230.pdf) and tried every possible pin configuration.

The problem is, that there is no signal on the receive pin, so there is no acknowledgement on the physical bus. If I set the CAN peripheral to Loopback mode, then the messages are transmitted, otherweise I will get an error.

The bus termination is correctly set with 2x 120 Ohm resistors on the ends.

The transceiver board is powered from the Arduino connector. I tried 3,3V (because it's a 3,3V transceiver) and 5V (transceiver is 5V tolerant), but there is no difference.

I'm using STM32CubeIDE v1.8.0 and STM32F7 MCU Package v1.16.2 (newest).

Does anyone have such issues with this board or any recommendations to solve this?

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
KnarfB
Super User

What CAN node(s) are on the bus? Only the STM32F769I-DISCO?

KnarfB

BViet.1
Associate III

The board is one node and another one is a PCAN-USB adapter with PCANView software.

You ever used CAN before?​

Transceiver used lots of places succesfully.

Would check schematic if the pins are conflicted.

Would check code for clocks being enabled, and rates/quanta matching the thing on the bus I'm talking at.

You need other devices on the bus to be responding when addressed..​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
BViet.1
Associate III

I'm very familar with CAN(FD) communication, but not with the STM32F769.

I implemented CAN-FD communication on an STM32H745 dual core and this works very well.

As i told the transmission works in Loopback mode, so I receive messages if the CAN TX pin is internal looped back to RX pin.

Also the transmission from PCAN to the board is not working. Because of this I think there is a problem on the board side.

Check the schematics and solder bridges, etc. PA11/PA12 sound like USB pins..

Check pins as GPIO toggling high/low.

Sorry don't know your history, first post..​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes it's my first post with this account. Have a new job, so my old account is not working anymore ;)

GPIO read and write on these pins are working as expected. I measured the output voltage levels with an oscilloscope and debugged the input levels during pin reading.

I've added a picture of the Arduino connector and the pinout of MCU.

0693W00000JOFbkQAH.png 0693W00000JOFd7QAH.png0693W00000JOFhTQAX.png

KnarfB
Super User

If you set CAN to normal mode, remove the transceiver, connect rx and tx with a wire, do you receive sent messages?

No I just see an ACK error.

Hello,

Did you connect Rs pin of the transceiver to the ground?

Check the power supply of the transceiver directly on pins 2 and 3.

SofLit

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.