STM32F769I-DISCO Using CAN interface over Arduino connector
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 1:44 AM
Hi,
I have a problem with CAN peripheral on this board. I tried the CAN Networking Example from the EVAL board and changed the pin configuration to fit to the Arduino connector.
I found some possible pin configurations:
CAN1_RX on PA11 -> D10
CAN1_TX on PA12 -> D13
CAN1_RX on PB8 -> D15
CAN1_TX on PB9 -> D14
I added an external transceiver from Waveshare (https://www.waveshare.net/w/upload/8/82/SN65HVD230.pdf) and tried every possible pin configuration.
The problem is, that there is no signal on the receive pin, so there is no acknowledgement on the physical bus. If I set the CAN peripheral to Loopback mode, then the messages are transmitted, otherweise I will get an error.
The bus termination is correctly set with 2x 120 Ohm resistors on the ends.
The transceiver board is powered from the Arduino connector. I tried 3,3V (because it's a 3,3V transceiver) and 5V (transceiver is 5V tolerant), but there is no difference.
I'm using STM32CubeIDE v1.8.0 and STM32F7 MCU Package v1.16.2 (newest).
Does anyone have such issues with this board or any recommendations to solve this?
- Labels:
-
CAN
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 3:16 AM
What CAN node(s) are on the bus? Only the STM32F769I-DISCO?
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 3:24 AM
The board is one node and another one is a PCAN-USB adapter with PCANView software.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 3:24 AM
You ever used CAN before?​
Transceiver used lots of places succesfully.
Would check schematic if the pins are conflicted.
Would check code for clocks being enabled, and rates/quanta matching the thing on the bus I'm talking at.
​
You need other devices on the bus to be responding when addressed..​
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 3:32 AM
I'm very familar with CAN(FD) communication, but not with the STM32F769.
I implemented CAN-FD communication on an STM32H745 dual core and this works very well.
As i told the transmission works in Loopback mode, so I receive messages if the CAN TX pin is internal looped back to RX pin.
Also the transmission from PCAN to the board is not working. Because of this I think there is a problem on the board side.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 3:40 AM
Check the schematics and solder bridges, etc. PA11/PA12 sound like USB pins..
Check pins as GPIO toggling high/low.
Sorry don't know your history, first post..​
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 3:51 AM
Yes it's my first post with this account. Have a new job, so my old account is not working anymore ;)
GPIO read and write on these pins are working as expected. I measured the output voltage levels with an oscilloscope and debugged the input levels during pin reading.
I've added a picture of the Arduino connector and the pinout of MCU.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 6:26 AM
If you set CAN to normal mode, remove the transceiver, connect rx and tx with a wire, do you receive sent messages?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-02 6:46 AM
No I just see an ACK error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-03 3:20 AM
Hello,
Did you connect Rs pin of the transceiver to the ground?
Check the power supply of the transceiver directly on pins 2 and 3.
SofLit