2019-03-12 7:46 PM
Hello, I am using the Stm32F769BI MCU.
I am receiving 3 ADC channels through DMA.
My problem is that debugging stops in the middle due to HAL_ADC_IRQHandler during debugging.
To debug again, I must press the Run button again.
I want to know why interrupts happen and stop. And I don't want to stop debugging in HAL_ADC_IRQHandler.
//adc
uint32_t air_adc_buf[3];
uint32_t adc_val[3];
/* USER CODE END 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
//buffer clear
for(int j = 0; j <=3; j++){
air_adc_buf[j] = 0;
}
if(hadc->Instance == ADC3)
{
adc_val[0] = air_adc_buf[0];
adc_val[1] = air_adc_buf[1];
adc_val[2] = air_adc_buf[2];
}
}
HAL_ADC_Start_DMA(&hadc3, &air_adc_buf[0], 3);
HAL_ADC_Start_IT(&hadc3);
while(1){
//adc
HAL_ADC_Start_IT(&hadc3);
printf("pressure sensor1 = %d\r\n", adc_val[0]);
printf("pressure sensor2 = %d\r\n", adc_val[1]);
printf("pressure sensor3 = %d\r\n", adc_val[2]);
printf("----------------\r\n");
HAL_Delay(500);
}
///////////
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hadc->Instance==ADC3)
{
/* USER CODE BEGIN ADC3_MspInit 0 */
/* USER CODE END ADC3_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_ADC3_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
/**ADC3 GPIO Configuration
PF8 ------> ADC3_IN6
PF9 ------> ADC3_IN7
PF10 ------> ADC3_IN8
*/
GPIO_InitStruct.Pin = S_ADC_0_Pin|S_ADC_1_Pin|S_ADC_2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
/* ADC3 DMA Init */
/* ADC3 Init */
hdma_adc3.Instance = DMA2_Stream0;
hdma_adc3.Init.Channel = DMA_CHANNEL_2;
hdma_adc3.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc3.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc3.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc3.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc3.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc3.Init.Mode = DMA_CIRCULAR;
hdma_adc3.Init.Priority = DMA_PRIORITY_LOW;
hdma_adc3.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_adc3.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;
hdma_adc3.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_adc3.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_adc3) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc3);
/* ADC3 interrupt Init */
HAL_NVIC_SetPriority(ADC_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(ADC_IRQn);
/* USER CODE BEGIN ADC3_MspInit 1 */
/* USER CODE END ADC3_MspInit 1 */
}
}
2019-03-12 7:46 PM
2019-03-12 7:47 PM
2019-03-15 9:07 AM
Hello,
Try to remove the printf function.
Best regards,
Mohamed aymen.
2019-03-15 9:40 AM
A few things:
(1) Your HAL_ADC_ConvCpltCallback() function is writing past the end of your air_adc_buf[] array. The array has 3 elements (0 to 2), but your for() loop goes from 0 to 3 (inclusive). Change "<= 3" to "< 3".
And a better (more maintainable) coding practice, make the array size a define and use that define everywhere. For example:
#define ADC_BUFFER_LEN 3
//adc
uint32_t air_adc_buf[ADC_BUFFER_LEN];
uint32_t adc_val[ADC_BUFFER_LEN];
And later:
/* USER CODE END 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
//buffer clear
for(int j = 0; j < ADC_BUFFER_LEN; j++){
air_adc_buf[j] = 0;
}
And still later:
HAL_ADC_Start_DMA(&hadc3, &air_adc_buf[0], ADC_BUFFER_LEN);
HAL_ADC_Start_IT(&hadc3);
(2) Why are you calling BOTH HAL_ADC_Start_DMA() and HAL_ADC_Start_IT()? Pick one or the other, I'm guessing the DMA version.
(3) Why do you clear air_adc_buf[] in the conversion complete callback, and then assign values from that array (which are zero) to adc_val[]? It seems you will always get zeros in adc_val[], no?