STM32F767 Window Watchdog Initialize Problem (System Always Get Reset)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
โ2025-03-18 12:49 AM
Hi for everyone,
I try to implement window watchdog to my system. I got reset every single time during enabling watchdog in HAL_WWDG_Init() function and exactly WRITE_REG(hwwdg->Instance->CR, (WWDG_CR_WDGA | hwwdg->Init.Counter)); here.
These are my watchdog configuration
hwwdg.Instance = WWDG;
hwwdg.Init.Prescaler = WWDG_PRESCALER_8;
hwwdg.Init.Window = 64;
hwwdg.Init.Counter = 127;
hwwdg.Init.EWIMode = WWDG_EWI_DISABLE;
I want to start watchdog and feed periodically but now, I just got reset and even dont even initialize successfully. It is default init function of library as you know. What should I do to successfully initialize Watchdog, feed it periodically, and ensure it runs properly?
I will be grateful for your help.
- Labels:
-
IWDG-WWDG
-
STM32CubeMX
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
โ2025-03-18 5:22 AM
Here is an example WWDG usage. I'd recommend getting that up and running.
Unlike the IWDG, the WWDG requires you to refresh it within a particular window. If you refresh outside of that window, it will reset. In your program, how do you ensure you're refreshing within that window?
The code presented looks fine.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
โ2025-03-18 5:36 AM
Thanks for reply.
I tried the example already but I am facing a problem in init function
HAL_StatusTypeDef HAL_WWDG_Init(WWDG_HandleTypeDef *hwwdg)
{
/* Check the WWDG handle allocation */
if (hwwdg == NULL)
{
return HAL_ERROR;
}
/* Check the parameters */
assert_param(IS_WWDG_ALL_INSTANCE(hwwdg->Instance));
assert_param(IS_WWDG_PRESCALER(hwwdg->Init.Prescaler));
assert_param(IS_WWDG_WINDOW(hwwdg->Init.Window));
assert_param(IS_WWDG_COUNTER(hwwdg->Init.Counter));
assert_param(IS_WWDG_EWI_MODE(hwwdg->Init.EWIMode));
#if (USE_HAL_WWDG_REGISTER_CALLBACKS == 1)
/* Reset Callback pointers */
if (hwwdg->EwiCallback == NULL)
{
hwwdg->EwiCallback = HAL_WWDG_EarlyWakeupCallback;
}
if (hwwdg->MspInitCallback == NULL)
{
hwwdg->MspInitCallback = HAL_WWDG_MspInit;
}
/* Init the low level hardware */
hwwdg->MspInitCallback(hwwdg);
#else
/* Init the low level hardware */
HAL_WWDG_MspInit(hwwdg);
#endif /* USE_HAL_WWDG_REGISTER_CALLBACKS */
/* Set WWDG Counter */
WRITE_REG(hwwdg->Instance->CR, (WWDG_CR_WDGA | hwwdg->Init.Counter));
/* Set WWDG Prescaler and Window */
WRITE_REG(hwwdg->Instance->CFR, (hwwdg->Init.EWIMode | hwwdg->Init.Prescaler | hwwdg->Init.Window));
/* Return function status */
return HAL_OK;
}
WRITE_REG(hwwdg->Instance->CR, (WWDG_CR_WDGA | hwwdg->Init.Counter)); line reset the system.
I created a timer to periodically refresh the watchdog every 20 seconds, but the main problem is I cannot skip wwdg_init successfully. I get reset just after enabling watchdog. My APB1 peripheral clock is 54 MHz. (maximum speed)
hwwdg.Instance = WWDG; hwwdg.Init.Prescaler = WWDG_PRESCALER_8; hwwdg.Init.Window = 64; hwwdg.Init.Counter = 127; hwwdg.Init.EWIMode = WWDG_EWI_DISABLE;
and there is my watchdog configuration. What can I do now in this situation? Waiting for your answers.