2020-07-27 7:43 AM
Hello ;
I am trying to test usart DMA on F7 . I only can transmite one time ; when i call usart init again its ok . but i still could not understand why .
Could you help please
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(500);
/* Get the CR register value */
HAL_UART_Transmit_DMA(&huart6, text, 21);
/* USART6 DMA Init */
/* USART6_TX Init */
//HAL_UART_Transmit_DMA(&huart6, text, 21);
}
/* USER CODE END 3 */
}
Thank you
2020-07-27 10:54 AM
Check for completion, check for error/status returned by function.
If processor stuck, break in with debugger and determine where. Is it expecting interrupt and callback functions to be implemented?