2015-08-22 4:24 PM
Hello Everyone.
As the title suggest, I am trying to receive data from the two digital microphones that are on the STM32F7 discovery board. Since the microphones are connected to the audio codec, I need to interface with the code to receive the data. I am using DMA to automatically transfer the data from SAI to memory.
I have looked at the examples provided and have managed to get it to work partially.The problem is with the data received.
Here is a pic of the data I am getting when there is little to no sound
http://pasteboard.co/4uu899x.png
As you can see, it fluctuates between either really high or really low values.
Please see the attached file for code.
#stm32f7 #sai-audio-codec2015-08-23 4:24 AM
it's two's complement data, so all are really low values.
change your data watch window to signed.2015-08-23 7:26 AM
Thank you so much.
2015-09-23 2:03 PM
Have you managed to retrieve data from both microphones at once?
The codec for the audio processor looks like it only supports one microphone or line in.