cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446VET7 Two Float Value Difference Problem

testbenchmark
Associate III

 

void AltitudeBuffer_Write(AltitudeBuffer_t* AltitudeBuffer, float altitude) { static int i=0; i++; AltitudeBuffer->readTime[i%2] = FlightFlagTime.CurrentTime; uint32_t timeDifference = ( AltitudeBuffer->readTime[i%2] - AltitudeBuffer->readTime[(1 - (i%2))]); if( ((AltitudeBuffer->head+1)%ALTITUDE_BUFFER_SIZE ) == AltitudeBuffer->tail ) { float tempValue = 0; for(int i=0; i<10; i++) { tempValue += AltitudeBuffer->buffer[i]; } tempValue /= 10; AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2] = tempValue; AltitudeBuffer->avarageAltitude[2] = ( (AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2]) - (AltitudeBuffer->avarageAltitude[1-((AltitudeBuffer->tail) % 2)]) ); AltitudeBuffer->VerticalSpeed = abs((AltitudeBuffer->avarageAltitude[2] / timeDifference)*1000); AltitudeBuffer->tail = (AltitudeBuffer->tail + 1)%ALTITUDE_BUFFER_SIZE; } AltitudeBuffer->buffer[AltitudeBuffer->head] = altitude; AltitudeBuffer->head = ( (AltitudeBuffer->head + 1) % ALTITUDE_BUFFER_SIZE ); }

 

in line 16 ; 

when (tail%2) = 0 

AltitudeBuffer->avarageAltitude[2] = ( (AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2]) - (AltitudeBuffer->avarageAltitude[1-((AltitudeBuffer->tail) % 2)]) );  is negative.

For example I got this values in debug session ; 

(AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2]) is = 897.060547

(AltitudeBuffer->avarageAltitude[1-((AltitudeBuffer->tail) % 2)]) is = 868.588684

so

AltitudeBuffer->avarageAltitude[2] should be = 897.060547 - 868.588684 = 28.471863

but it is oppiste of this value. I got ;

AltitudeBuffer->avarageAltitude[2] = -28.4718628

 

When tail % 2 = 0 its negative When tail % 2 = 0 its positive

but eitherway (AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2])

is bigger than

(AltitudeBuffer->avarageAltitude[1-((AltitudeBuffer->tail) % 2)]);

 

or example when tail % 2 = 1

(AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2]) is = 1.18015742

and

(AltitudeBuffer->avarageAltitude[1-((AltitudeBuffer->tail) % 2)]) is = 1.11249995

AltitudeBuffer->avarageAltitude[2] = 0.0676574707

Can u help me please?

I tried with double types instead of float but its not worked. I cannot define the problem exactly

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Okay, showing all variables, good, but you've cropped it so we can't see where execution is at when those expressions are evaluated. Note that "tail" is also modified in the given code. Set a breakpoint at the "AltitudeBuffer->avarageAltitude[2] =" line, and step over. If you do that, only the "AltitudeBuffer->avarageAltitude[2]" will show up with a red background, instead of everything, indicating it (and only it) was changed since the last break.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

7 REPLIES 7
TDK
Guru

Let's be objective here. The processor is unlikely to be performing math incorrectly. It's handled in hardware by the core, which is used by millions of people and doesn't have glaring issues. Similarly, the compiler is also widely used and is unlikely to be creating the incorrect assembly code. So what's left?

  • Perhaps you are mistaken in what values are what. Try to capture everything in a screenshot rather than cut/paste which is subject to translation errors.
  • Perhaps this is a temporal issue. Put a breakpoint after the "invalid" statements are executed and show the values in the expression window.
If you feel a post has answered your question, please click "Accept as Solution".

Hi TDK, 

Thank you for answering

testbenchmark_0-1724685185209.png

Tail is = 9 

it means Tail%2 = 1

AltitudeBuffer->avarageAltitude[AltitudeBuffer->tail % 2]

means = AltitudeBuffer->avarageAltitude[1]

and 

AltitudeBuffer->avarageAltitude[1-((AltitudeBuffer->tail) % 2)] 

means = AltitudeBuffer->avarageAltitude[0] 

 

AltitudeBuffer->avarageAltitude[0] = 962.237976

AltitudeBuffer->avarageAltitude[1] = 976.578308

 

AltitudeBuffer->avarageAltitude[2] = AltitudeBuffer->avarageAltitude[1] = 976.578308 - 962.237976 = 14.340332

But I got -14.340332

 

With screen shots :

testbenchmark_0-1724685656746.png

testbenchmark_1-1724685677203.png

testbenchmark_2-1724685696283.png

 

TDK
Guru

Okay, showing all variables, good, but you've cropped it so we can't see where execution is at when those expressions are evaluated. Note that "tail" is also modified in the given code. Set a breakpoint at the "AltitudeBuffer->avarageAltitude[2] =" line, and step over. If you do that, only the "AltitudeBuffer->avarageAltitude[2]" will show up with a red background, instead of everything, indicating it (and only it) was changed since the last break.

If you feel a post has answered your question, please click "Accept as Solution".

You change tail after the subtraction. When the difference was calculated, tail was 8.

JW

Hi TDK, Thank you for answering

I did what you said and you are right. When I add a breakpoint at this 3 lines I see it clearly.

Now tail is 7 and tail%2 = 1

its gonna be >> 0.19411011 - 0.251983643 = -0.0578735322

 

testbenchmark_1-1724697130675.png

testbenchmark_2-1724697278973.png

I am gonna try to fix that

Glad you figured it out.

Always good to simplify things when debugging to isolate the error. As a general rule, it's incredibly unlikely that the core or the compiler is the source of the issue. If you suspect one of those, try to prove it with a simple program and screenshots. Usually that convinces you otherwise and helps you find the misunderstanding. Works well for me anyway.

If you feel a post has answered your question, please click "Accept as Solution".