2020-06-16 4:23 AM
Hello All,
We have an custom board using stm32f446re controller which has 6 PIN SWD JTAG connector.
We are using NUCLEO-F446RE kit as debugger to flash the custom board as explained in "6.2.4 Using ST-LINK/V2-1 to program and debug an external STM32 application" from below link,
Removed CN2 jumpers
Connected CN4 SWD pins of NUCLEO-F446RE to custom SWD connector as appropriate signals.
But we are not flash or debug as we are getting below error in System workbench for STM32 IDE,
Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 480 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 480 kHz
Info : STLINK v2 JTAG v31 API v2 SWIM v7 VID 0x0483 PID 0x3748
Info : using stlink api v2
Info : Target voltage: 3.223483
Info : Stlink adapter speed set to 480 kHz
Info : STM32F446RETx.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: timed out while waiting for target halted
TARGET: STM32F446RETx.cpu - Not halted
in procedure 'reset'
in procedure 'ocd_bouncer'
Info : device id = 0x10006421
Warn : STM32 flash size failed, probe inaccurate - assuming 512k flash
Info : flash size = 512kbytes
Error: Target not halted
Error: failed erasing sectors 0 to 0
Error: flash_erase returned -304
Cross verified the FLASH SIZE and it's 512KB.
Can someone help here to understand the issue?
2020-06-16 6:24 AM
Use a short cable for the interconnection, max. 15cm.
JW