2023-11-15 2:49 AM
Hi
I try to implement the read protection on my STM32F44 board based on this example:
https://community.st.com/t5/stm32-mcus/how-to-change-the-read-out-protection-on-stm32f4/ta-p/49410
In principle, it works, but I have some strange behavior. My code:
if (level == 0x00 || level == 0x01) {
FLASH_OBProgramInitTypeDef pOBInit = { 0 };
HAL_FLASHEx_OBGetConfig(&pOBInit);
pOBInit.Banks = FLASH_BANK_1;
pOBInit.OptionType = OPTIONBYTE_RDP;
if (level == 0x00) {
new_level = OB_RDP_LEVEL_0;
}
else {
new_level = OB_RDP_LEVEL_1;
}
if (new_level != pOBInit.RDPLevel) {
do {
//Unlock flash
status = HAL_FLASH_Unlock();
//Unlock flash option sections
status = HAL_FLASH_OB_Unlock();
pOBInit.RDPLevel = new_level;
status = HAL_FLASHEx_OBProgram(&pOBInit);
//Triggers a reset
status = HAL_FLASH_OB_Launch();
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
printLogWarning(halToCANxError(status), "Writing flash read protection failed");
return 0;
} while (0);
//Something failed, flash maybe already unlocked
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
}
}
Two points are not working as they should:
Any idea what I can do to solve these issues, especially the second?
Thank you.
Solved! Go to Solution.
2023-11-15 3:29 AM
Hello @Corono ,
if the reset is done while the flash memory is not fully erased the RDP level will stay in level one this is explained in the example your trying to execute :
"if you reset the microcontroller before the FLASH memory is fully erased the RDP byte will stay locked at Level 1 and your program will be deleted, so it is very important so stand still while the FLASH is being mass erased."
so make sure you wait the appropriate time which can take upward of 20 Seconds . also don't forget to remove the CN2 connection of the STlink as referred in the example and after that you can check if the RDP level is set by reconnecting the jumpers and connecting via CubeProgrammer to verify .
BR
2023-11-15 3:07 AM
I solved the second problem. Because the reset didn't work correctly, I added a manual reset (not in the code above). However, it seems that the MCU was reset to early and the flag was not removed properly. If I remove the manual reset, disabling works.
2023-11-15 3:29 AM
Hello @Corono ,
if the reset is done while the flash memory is not fully erased the RDP level will stay in level one this is explained in the example your trying to execute :
"if you reset the microcontroller before the FLASH memory is fully erased the RDP byte will stay locked at Level 1 and your program will be deleted, so it is very important so stand still while the FLASH is being mass erased."
so make sure you wait the appropriate time which can take upward of 20 Seconds . also don't forget to remove the CN2 connection of the STlink as referred in the example and after that you can check if the RDP level is set by reconnecting the jumpers and connecting via CubeProgrammer to verify .
BR
2023-11-15 5:17 AM
Thank you for your answer. Understood.
For me, the behavior of the function "HAL_FLASH_OB_Launch()" is still a bit strange. What I observed:
However, I can handle this in the code and the module is not reset.
2023-11-15 6:06 AM
Hello @Corono ,
how can you confirm that code execution in not stopped after HAL_FLASH_OB_Launch() in the level changed from 0 to 1 (without debugger) case ? this should not be possible because as you said this should trigger the flash erase process so i want to know how you identified that the code is still working .
BR
2023-11-15 7:43 AM
A change from OB_RDP_LEVEL_1 to OB_RDP_LEVEL_0 triggers the flash erase, not the other way around.
A change from OB_RDP_LEVEL_0 to OB_RDP_LEVEL_1 enables the read protection. In this case (without debugger), there is no restart. I have a log message after HAL_FLASH_OB_Launch() and this message is sent. And the module stays in operation and is responding to commands it wouldn't after a restart.