cancel
Showing results for 
Search instead for 
Did you mean: 

Upload .bin files on windowsthrough the USB interface

Elijah1
Associate

Hi, I just decided to try mbed OS 6 for programming my NUCLEO-WB15CC. Compilation is successful, but when i try to flash the compiled .bin file, the operation fails saying that a device was not connected even though it was. I am guessing it is because my board does not show up as shown here http://imgur.com/a/h2th7 (source : another post on another forum, referenced below)

So I have two questions.

1) Why cannot I flash my board directly from MBED CLI ? is it because the board does not appear as a USB drive ?

2) Is there any way to show my device as a usb device as shown in the picture so that I can at least drag and drop the .bin ? I tried installing the driver mentioned in the solution here. The installation was successful, but it did not solve my problem.

Any help in resolving this will be appreciated. Thank you.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0