cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f429i_disc1 BSP_LCD_DrawBitmap

Franksterb92
Senior

im having trouble displaying my own bitmap what converter should i use to convert a bmp file to array to work with this function 

1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi @Franksterb92 ,

Some converters may be used to convert the input image to a C or a header file.

In AN4861, "LCD image converter tool" is used to generate required input file.

You can refer to the paragraph "Display an image from the internal flash" for more details.

-Amel

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee

Hi @Franksterb92 ,

Some converters may be used to convert the input image to a C or a header file.

In AN4861, "LCD image converter tool" is used to generate required input file.

You can refer to the paragraph "Display an image from the internal flash" for more details.

-Amel

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

thank you for the help st is the best!!!!!!!!!!!!