cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 Communication with STM32F401 use SPI, the slave data shift.

WBowe
Associate II

board: STM32F429I-DISC1

NUCLEO-F401RE

I use SPI with DMA , but the MOSI will shift randomly.

​

Connection of two boards.

0690X00000AqTH0QAN.png

Master(STM32F429)

void init_SPI1(void)
{
	GPIO_InitTypeDef GPIO_InitStruct;
	SPI_InitTypeDef SPI_InitStruct;
	RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
	RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
	GPIO_InitStruct.GPIO_Pin = GPIO_Pin_5| GPIO_Pin_6 | GPIO_Pin_7;
	GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
	GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
	GPIO_Init(GPIOA, &GPIO_InitStruct);
	GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9 ;//Select Chip
	GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;
	GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;
	GPIO_Init(GPIOD, &GPIO_InitStruct);
	GPIO_InitStruct.GPIO_Pin =  GPIO_Pin_4 ;//Select Chip
	GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;
	GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;
	GPIO_Init(GPIOA, &GPIO_InitStruct);
	GPIO_SetBits(GPIOA, GPIO_Pin_4);//For stm32f429 discovery board
	GPIO_SetBits(GPIOD, GPIO_Pin_9);//For stm32f401 manual board
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);
	SPI_I2S_DeInit(SPI1);
	SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
	SPI_InitStruct.SPI_Mode = SPI_Mode_Master;
	SPI_InitStruct.SPI_DataSize = SPI_DataSize_16b;
	SPI_InitStruct.SPI_CPOL = SPI_CPOL_High;
	SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
	SPI_InitStruct.SPI_NSS = SPI_NSS_Soft|SPI_NSSInternalSoft_Set ;
	SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8  ;
	SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
  SPI_InitStruct.SPI_CRCPolynomial = 7;
	SPI_Init(SPI1, &SPI_InitStruct);
	
	SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE);	
	NVIC_InitTypeDef NVIC_InitStructure;
	NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn; 
	NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
	NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; 
	NVIC_InitStructure.NVIC_IRQChannelCmd = DISABLE;
	NVIC_Init(&NVIC_InitStructure);
	
  SPI_Cmd(SPI1, ENABLE);
}
 
void Finger_Connect(uint16_t mode)
{
	GPIO_ResetBits(GPIOA, GPIO_Pin_4);
	GPIO_ResetBits(GPIOD, GPIO_Pin_9);
 
		while(SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE) == RESET);
		SPI_I2S_SendData(SPI1,mode);
		while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
		SPI_Buffer_Rx[0] = SPI_I2S_ReceiveData(SPI1);
	
	for(int i = 0 ; i <spirecivetime ; i++){
		while(SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE) == RESET);
		SPI_I2S_SendData(SPI1,0xAAAA);
		while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
		SPI_Buffer_Rx[i+1] = SPI_I2S_ReceiveData(SPI1);
	}
	GPIO_SetBits(GPIOA, GPIO_Pin_4);
	GPIO_SetBits(GPIOD, GPIO_Pin_9);
}

​Slave(STM32F401)

uint16_t SEND_BUFF[15]={0x5555,0xAAAA,0x1234,0x2345,0x3456,0x4567,0x5678,0x6789,0,0,0,0,0,0,0}, RECEIVE_BUFF[15]={0};
 
void init_SPI1(void)
{
	GPIO_InitTypeDef GPIO_InitStruct;
	SPI_InitTypeDef SPI_InitStruct;
	DMA_InitTypeDef DMA_InitStructure;
	NVIC_InitTypeDef NVIC_InitStructure;	
	RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
	RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
	RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
	
	GPIO_InitStruct.GPIO_Pin = GPIO_Pin_4| GPIO_Pin_5| GPIO_Pin_6 | GPIO_Pin_7;
	GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
	GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
	GPIO_Init(GPIOA, &GPIO_InitStruct);
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI1);
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);
	SPI_I2S_DeInit(SPI1);
	SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; 
	SPI_InitStruct.SPI_Mode = SPI_Mode_Slave;
	SPI_InitStruct.SPI_DataSize = SPI_DataSize_16b;
	SPI_InitStruct.SPI_CPOL = SPI_CPOL_High;
	SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
	SPI_InitStruct.SPI_NSS = SPI_NSS_Hard ;
	SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
	SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
  SPI_InitStruct.SPI_CRCPolynomial = 7;
	SPI_Init(SPI1, &SPI_InitStruct);
 
	/* SPI_MASTER_Rx_DMA_Channel configuration ---------------------------------*/
	DMA_DeInit(DMA2_Stream2);
	DMA_DeInit(DMA2_Stream5);
 
	DMA_StructInit(&DMA_InitStructure);
	DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(&(SPI1->DR));
	DMA_InitStructure.DMA_BufferSize = SPI_BUFFERSIZE;
	DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
	DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
	DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
	DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
	DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
	DMA_InitStructure.DMA_Priority = DMA_Priority_High;
	DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
	DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_1QuarterFull ;
	DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single ;
/* SPI_MASTER_Rx_DMA_Channel configuration ---------------------------------*/
	DMA_InitStructure.DMA_Channel = DMA_Channel_3; 
	DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;					
	DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)RECEIVE_BUFF;
	DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
	DMA_Init(DMA2_Stream2, &DMA_InitStructure);
	DMA_Cmd(DMA2_Stream2, DISABLE);
	
	/* SPI_MASTER_Tx_DMA_Channel configuration ---------------------------------*/
	DMA_InitStructure.DMA_Channel = DMA_Channel_3;
	DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
	DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)SEND_BUFF;
	DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral;
	DMA_Init(DMA2_Stream5, &DMA_InitStructure);
	DMA_Cmd(DMA2_Stream5, DISABLE);	
	
	NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream5_IRQn;
	NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
	NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
	NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
	NVIC_Init(&NVIC_InitStructure);
	
	NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream2_IRQn;
	NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
	NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;
	NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
	NVIC_Init(&NVIC_InitStructure);
	
	DMA_ClearFlag(DMA2_Stream2, DMA_FLAG_TCIF2);
	DMA_ClearFlag(DMA2_Stream5, DMA_FLAG_TCIF5);
	
	DMA_ITConfig(DMA2_Stream2, DMA_IT_TC , ENABLE);
	DMA_ITConfig(DMA2_Stream5, DMA_IT_TC , ENABLE);
	
	DMA_Cmd(DMA2_Stream2, ENABLE);
	DMA_Cmd(DMA2_Stream5, DISABLE);	
	/* Enable SPI_MASTER DMA Tx request */
	SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Tx, ENABLE);
	/* Enable SPI_MASTER DMA Rx request */
	SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Rx, ENABLE);
	SPI_Cmd(SPI1, ENABLE);
}
void DMA2_Stream5_IRQHandler(void)
{
	if(DMA_GetITStatus(DMA2_Stream5, DMA_IT_TCIF5) == SET)
	{
		DMA_ClearITPendingBit(DMA2_Stream5, DMA_IT_TCIF5);
	}
}
void DMA2_Stream2_IRQHandler(void)
{
	if(DMA_GetITStatus(DMA2_Stream2, DMA_IT_TCIF2) == SET)
	{
		DMA_ClearITPendingBit(DMA2_Stream2, DMA_IT_TCIF2);
		DMA2_Stream5->NDTR = 15;		
		DMA_Cmd(DMA2_Stream5, ENABLE);
	}
}

Random capture by logic analyzer

0690X00000AqTOfQAN.png

0690X00000AqTO6QAN.png0690X00000AqTO7QAN.pngI try the setting in Slave by change the configuration hard chip select and soft chip select, and the situation is the same.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

> GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;

Use lower OSPEEDR setting, shorter interconnection, twist the SCK with a ground wire.

JW

I try to twist the SCK with a ground wire, it can success communication in soft chip select.

But when I change the setting the MISO also shift in hard chip select.

waclawek.jan
Super User

Use lower OSPEEDR setting