2016-03-28 02:29 PM
Recently the STM32F407 discovery board changed part numbers from STM32F4DISCOVERY to STM32F407G-DISC1. The old boards could be powered directly via the 5V pins on the headers, or via a USB wall-wart, but the new boards need to be connected to a PC in order to boot. Is this intended behavior? Is there a solution aside from flashing an older firmware to the STLink chip?
Thanks #stm32f407g-disc12016-03-28 03:59 PM
I think it has been discussed or documented. I don't think you can get the older model firmware on the ST-LINK easily.
Check SB11 (NRST)http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00039084.pdf
2016-04-05 10:18 AM
Hi trent,
You should upgrade your ST-LINK firmware to ST-LINK/V2-1 through
http://www.st.com/web/en/catalog/tools/PF260217
.-Hannibal-
Recently the STM32F407 discovery board changed part numbers from STM32F4DISCOVERY to STM32F407G-DISC1. The old boards could be powered directly via the 5V pins on the headers, or via a USB wall-wart, but the new boards need to be connected to a PC in order to boot. Is this intended behavior? Is there a solution aside from flashing an older firmware to the STLink chip?
Thanks2017-11-10 11:14 AM
2017-11-10 02:05 PM
You have a different issue from the one reported by the OP