2023-01-28 6:46 PM
Most of the future time occurs around 12:00 in the morning, here are the instances captured on the device:
1. The actual time is: 2023-01-11 11:59:55, the STM32F407 RTC time is: 2023-01-12 12:00:00
2. The actual time is: 2022-12-31 11:59:58, the STM32F407 RTC time is: 2023-01-01 12:00:00
Under normal circumstances, the actual time and the STM32F407 RTC time do not exceed plus or minus 10s
2023-01-28 8:04 PM
How do you read it time in your program?
Read it and check/post RTC registers' content.
JW
2023-01-30 9:40 PM
The program will read the RTC value many times a second, or read the RTC value only once in a few seconds, and then upload the RTC time and other information to the server in real time through the network, and the server will regularly compare the local time with the uploaded RTC time. future time
2023-01-31 5:59 AM
Read out and check/post content of RTC registers.
Maybe consequence of using uninitialized structs when setting time/date, e.g. as here.
JW
2023-02-01 7:34 PM
We are using a 24-hour system, and a small number of devices are at 11:59:59 am today, and the next moment becomes 12:00:00 tomorrow, and it will not return to normal until the next time synchronization
set the rtc time as follow:
/* Get the RTC current Time */
HAL_RTC_GetTime(&hrtc, &stimestructureget, RTC_FORMAT_BIN);
/* Get the RTC current Date */
HAL_RTC_GetDate(&hrtc, &sdatestructureget, RTC_FORMAT_BIN);
stimestructureget.Hours = tm_p->tm_hour;
stimestructureget.Minutes = tm_p->tm_min;
stimestructureget.Seconds = tm_p->tm_sec;
sdatestructureget.Year = tm_p->tm_year - 100;//-1900
sdatestructureget.Month = tm_p->tm_mon + 1;
sdatestructureget.Date = tm_p->tm_mday ;
sdatestructureget.WeekDay = tm_p->tm_wday + 1;
PRINTF("get time:%u-%u-%u %u:%u:%u\n",tm_new.tm_year,tm_new.tm_mon,tm_new.tm_mday,tm_new.tm_hour,tm_new.tm_min,tm_new.tm_sec);
/* Set the RTC current Time */
HAL_RTC_SetTime(&hrtc, &stimestructureget, RTC_FORMAT_BIN);
/* Set the RTC current Date */
HAL_RTC_SetDate(&hrtc, &sdatestructureget, RTC_FORMAT_BIN);
The RTC initialization configuration is as follows:
void MX_RTC_Init(void)
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initialize RTC and set the Time and Date
*/
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2);
}
}
2023-02-02 3:28 AM
Read out and check/post content of RTC registers. Do it. You'll be surprised.
In MX_RTC_Init() you don't set the sTime.TimeFormat before calling HAL_RTC_SetTime(). Set it, or, maybe better, initialize the structs when defining them:
RTC_TimeTypeDef sTime = {0};
RTC_DateTypeDef sDate = {0};
JW