cancel
Showing results for 
Search instead for 
Did you mean: 

Error in Final Launch Sequence

Nico3
Senior

I am trying to upload the code to my target STM32F407 but below error is showing up. I tried some of suggestions but problem is still there. I am using Version: 1.15.1.   Debug log file also attached. 

1) Doing Mass Erase of flash,

2) Updating ST Link Firmware

3) Set Reset Behavior: None

4) Uncheck Enable Live Expressions

Nico3_0-1720244408387.png

 

Update:   I moved to STM32Cube programmer instead of using STM32cubeide, and able to upload the code after reducing ST-Link Frequency to 15Khz. Is it due to my target board poor design or something else. I am using Discovery Board ST-LINK to upload

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Nico3
Senior

 Pls note issue has been solved. The problem was with jumper cables between ST-LINK and Target board. We used new cables and all in single ribbon, so now it is working fine.  

I conclude EMI was issue..

View solution in original post

3 REPLIES 3
Nico3
Senior

 Pls note issue has been solved. The problem was with jumper cables between ST-LINK and Target board. We used new cables and all in single ribbon, so now it is working fine.  

I conclude EMI was issue..

chau
Associate

i downloaded and installed STM32 ST-LINK Utility. Then I erase chip by STM32 ST-LINK Utility. Then I open program in Stm32Cube and run program with stm32 board. It works. 

@chau  Note that the old ST-Link Utility is long obsolete - although it may still work with older parts (like the F407 here), it's not going to help for newer ones.

As the OP said, STM32CubeProgrammer is the way forward.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.