2016-02-25 2:16 AM
Hello,
One of the requirement for my project is to log diagnostic data periodically over a period of time.
Controller used is STM32F405xx, LQFP64. As it does not have the on chip EEPROM, I want to interface (via SPI) externally.
As per my customer requirement, Diagnostic data and raw data to be logged for every 20 minutes. For one year backup, I need 6.727Mbit (each data set 32 bytes) and write cycles are 26280.
Concern:
I found EEPROM from ST � �M95M02-DRMN6TP�. Size is only 2Mbits and cost is around $1.5
Even for 6 months data backup also, this is very high cost (>$3) solution for target price of product.
There are other type memories � NAND flash/NOR Flash which are very cheap. Endurance and Retention time are very less than EEPROM, but looks feasible for my requirement.
-
Are there any other dis-advantages of Flash memory?
-
Is there any low cost solution from ST products? Preferably <$1.
I have read lot of material from on-line, but couldn�t able to conclude. Kindly suggest.
Regards,
Govind.
#eeprom #spi #stm32f405xx2016-02-25 6:03 AM
I'd probably look at an SPI Flash, and the internal Flash of the STM32 itself as your requirements wouldn't seem to stress that.
The other alternative might be a MicroSD card.You might also want to determine if your data is compressible.2016-02-25 7:16 PM
Admittedly not an ST product, but e.g. Digikey are offering 8Mbit Spansion S25FL208 SPI Flash in SOIC8 package for AU$0.55 in single units.
2016-02-28 11:24 PM
Dear rao_k.govinda,
Best solution is to use MicroSd Card. Would be cheap, easy to use and you can use a file system supported on multi platforms also(like windows). Data recovery is easy.
/
*Please
mark helpfull
if this post helps you or solves your problem.*/
/* If you need any personal support for your work please contact at
embeddeddesign.help@gmail.com*/