cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F405 About recovery from standby mode. Is there any way to recover from standby mode with UART reception?

TKTKTK
Associate

Is it possible to wake up by connecting the UART pins in PWR_EnterSTOPMode to the pins used for wake up?

1 ACCEPTED SOLUTION

Accepted Solutions
Piranha
Chief II

So are you asking about Standby or Stop mode? And the wake-up pins can wake up the MCU from any mode.

View solution in original post

2 REPLIES 2
Piranha
Chief II

So are you asking about Standby or Stop mode? And the wake-up pins can wake up the MCU from any mode.

S.Ma
Principal

In STM32L products can be found LPUART which can wakeup from low power mode without losing the first incoming byte.