cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 NUCLEO-F429ZI Unable to Communicate with HMI via RS232/RS485

QuangIoT
Associate II

 

I am facing an issue connecting the STM32F4 NUCLEO-F429ZI board to an HMI screen that uses RS232 and RS485 communication standards. The HMI can communicate successfully with my computer, but the STM32 board cannot communicate with the computer except through UART3 and using a direct cable connection. This prevents me from establishing communication between the STM32 board and the HMI screen.

Could you please help me identify what might be causing this issue and how I can resolve it?

Thank you!

1 ACCEPTED SOLUTION

Accepted Solutions

@QuangIoT wrote:

I'm using this cable and i ensure correct communication standard


That's the USB cable which connects the ST-Link to your computer.

That's what carries the debug/programming connection, and the VCP (Virtual COM Port)

As pointed out by @mƎALLEm, that VCP is connected to USART3 (PD8 & PD9) on the STM32F4 microcontroller.

So, if you want to use USART3 to communicate with any external device, you are first going to have to disconnect it from the ST-Link VCP - that's what the SB5 & SB6 links are for:

AndrewNeil_0-1732614281721.png

AndrewNeil_1-1732614678241.png

https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdf#page=1

AndrewNeil_2-1732614918993.png

 

 

Of course, once you've disconnected them from the ST-Link, then you will no longer be able to communicate over the VCP - you will need a separate USB-to-UART converter.

Similarly, if you use any other UART connection than PD8 & PD9, that will not be connected to the ST-Link and, therefore, will not be accessible via the ST-Link's VCP -  so you will, again, need a separate USB-to-UART converter.

 

View solution in original post

16 REPLIES 16
mƎALLEm
ST Employee

Hello @QuangIoT 

1- The thread is not related to STM32CubeIDE usage to put it in STM32CubeIDE forum board but to the usage of the MCU. Needs to be moved to "STM32 MCUs Products" forum board.

2- The information you provided are insufficient. Need to elaborate and give more details about the HW and the software and what you have tried at this stage.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I have connected the TX of the HMI to the RX of the MCU and vice versa, with GND shared, but data is not being transmitted or received.6a8e5e05-678a-4e3b-a39c-5ade608e53d7.jfif

Do you want me to provide anything else? Please give me a request


@QuangIoT wrote:

I have connected the TX of the HMI to the RX of the MCU and vice versa, with GND shared, but data is not being transmitted or received.


So, again, what investigation/testing/debugging have you done to find out what's going on?

  • Is your Nucleo actually transmitting anything at all? If so, is it transmitting correctly?
  • Does your Nucleo receive correctly?
  • Have you tested the parts separately - eg, with a terminal - before wiring them together?

 

Some tips here on debugging serial comms:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/tac-p/706966/highlight/true#M49

What do you mean by:


@QuangIoT wrote:

but data is not being transmitted or received.


What you have debugged at this level: in software and HW?

Did you probe Tx and Rx with a scope/logic analyzer? what did you find?

Need to provide more details: software, Hardware: schematics and so on .. When you said "HMI screen" what's its comm specification? datasheet?, what about your code?  etc etc ..

No one here have a crystal ball to give a direct answer.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
QuangIoT
Associate II

So, again 

I have tested the STM32 separately with the computer, but the STM32 does not receive the messages sent from the computer.
I have tried debugging both the hardware and software.
I'm using  DMG80480C070_15WTR display
Display Specifications
Resolution: 800x480 pixels
Screen Size: 7 inches
Display Type: TFT LCD with capacitive or resistive touchscreen options
Brightness: Typically 250–300 cd/m²
Viewing Angle: Wide-angle, usually 140° horizontal and 120° vertical
Electrical Specifications
Voltage: 5V DC
Current Consumption: Approximately 450mA
Backlight Lifetime: Typically 20,000–30,000 hours
Communication Interfaces
RS232: Supports serial communication
RS485: For industrial environments requiring differential signaling
TTL UART: 3.3V level UART communication
Baud Rate: Configurable, typically 9600 to 115200 bps
Memory
Flash Storage: Up to 16MB for interface and data storage
RAM: Internal, optimized for smooth GUI operation
Software and Features
Development Software: DWIN DGUS or DGUS II IDE
GUI Library: Supports variable display, image switching, sliders, data curves, and animations
File Format: Uses .bin files for firmware and GUI updates
Touch Support: Capacitive or resistive touch depending on the model
Data Protocol: Uses a customized protocol for communication between the screen and host MCU
Environmental Specifications
Operating Temperature: -20°C to 70°C
Storage Temperature: -30°C to 80°C
Humidity: 10% to 90% RH non-condensing
Dimensions
Outline Size: Approximately 165mm x 100mm x 15mm
Active Area: 154.08mm x 85.92mm
 

 

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "lwip.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart5;
UART_HandleTypeDef huart7;
UART_HandleTypeDef huart2;
UART_HandleTypeDef huart3;
UART_HandleTypeDef huart6;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_UART5_Init(void);
static void MX_USART6_UART_Init(void);
static void MX_UART7_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

uint8_t u8RxData[1] = {2};

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART3_UART_Init();
  MX_LWIP_Init();
  MX_USART2_UART_Init();
  MX_UART5_Init();
  MX_USART6_UART_Init();
  MX_UART7_Init();
  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

	  if (HAL_UART_Receive(&huart3, u8RxData, sizeof(u8RxData),1000) == HAL_OK){
	  HAL_UART_Transmit(&huart3, u8RxData, sizeof(u8RxData),1000);
	  }
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 180;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 4;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Activate the Over-Drive mode
  */
  if (HAL_PWREx_EnableOverDrive() != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief UART5 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_UART5_Init(void)
{

  /* USER CODE BEGIN UART5_Init 0 */

  /* USER CODE END UART5_Init 0 */

  /* USER CODE BEGIN UART5_Init 1 */

  /* USER CODE END UART5_Init 1 */
  huart5.Instance = UART5;
  huart5.Init.BaudRate = 115200;
  huart5.Init.WordLength = UART_WORDLENGTH_8B;
  huart5.Init.StopBits = UART_STOPBITS_1;
  huart5.Init.Parity = UART_PARITY_NONE;
  huart5.Init.Mode = UART_MODE_TX_RX;
  huart5.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart5.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart5) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN UART5_Init 2 */

  /* USER CODE END UART5_Init 2 */

}

/**
  * @brief UART7 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_UART7_Init(void)
{

  /* USER CODE BEGIN UART7_Init 0 */

  /* USER CODE END UART7_Init 0 */

  /* USER CODE BEGIN UART7_Init 1 */

  /* USER CODE END UART7_Init 1 */
  huart7.Instance = UART7;
  huart7.Init.BaudRate = 115200;
  huart7.Init.WordLength = UART_WORDLENGTH_8B;
  huart7.Init.StopBits = UART_STOPBITS_1;
  huart7.Init.Parity = UART_PARITY_NONE;
  huart7.Init.Mode = UART_MODE_TX_RX;
  huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart7.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart7) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN UART7_Init 2 */

  /* USER CODE END UART7_Init 2 */

}

/**
  * @brief USART2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{

  /* USER CODE BEGIN USART2_Init 0 */

  /* USER CODE END USART2_Init 0 */

  /* USER CODE BEGIN USART2_Init 1 */

  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */

  /* USER CODE END USART2_Init 2 */

}

/**
  * @brief USART3 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART3_UART_Init(void)
{

  /* USER CODE BEGIN USART3_Init 0 */

  /* USER CODE END USART3_Init 0 */

  /* USER CODE BEGIN USART3_Init 1 */

  /* USER CODE END USART3_Init 1 */
  huart3.Instance = USART3;
  huart3.Init.BaudRate = 115200;
  huart3.Init.WordLength = UART_WORDLENGTH_8B;
  huart3.Init.StopBits = UART_STOPBITS_1;
  huart3.Init.Parity = UART_PARITY_NONE;
  huart3.Init.Mode = UART_MODE_TX_RX;
  huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart3.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart3) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART3_Init 2 */

  /* USER CODE END USART3_Init 2 */

}

/**
  * @brief USART6 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART6_UART_Init(void)
{

  /* USER CODE BEGIN USART6_Init 0 */

  /* USER CODE END USART6_Init 0 */

  /* USER CODE BEGIN USART6_Init 1 */

  /* USER CODE END USART6_Init 1 */
  huart6.Instance = USART6;
  huart6.Init.BaudRate = 115200;
  huart6.Init.WordLength = UART_WORDLENGTH_8B;
  huart6.Init.StopBits = UART_STOPBITS_1;
  huart6.Init.Parity = UART_PARITY_NONE;
  huart6.Init.Mode = UART_MODE_TX_RX;
  huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart6.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart6) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART6_Init 2 */

  /* USER CODE END USART6_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOF_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, LED1_Pin|LED2_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pins : LED1_Pin LED2_Pin */
  GPIO_InitStruct.Pin = LED1_Pin|LED2_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */


 

 

At this level, forget about HMI and focus on the UART communication as you said:


@QuangIoT wrote:

So, again 

I have tested the STM32 separately with the computer, but the STM32 does not receive the messages sent from the computer.

Are you using USART3 with the computer over STLINK? what GPIOs you are using? PD8 and PD9?

SofLit_0-1732531726216.png

PS: the spec you provided doesn't give much information (for example mechanical information is useless). But anyway you need at least to achieve the communication between NUCLEO and the computer.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
QuangIoT
Associate II

I'm using USART 3 with my computer via STLINK and communication is normal, but if I switch to using USART2 (PD5 is TX and PD6 is RX) and of course the code will also change from uart3 to uart2 but it won't transmit. receive. During that process, I still have the transmission cable plugged in. Is there any problem that will cause me to not be able to transmit or receive data with uart2?