2018-12-14 2:03 AM
I'm working over STM32f334, i config cubeMx to use TIM6 o TIM7 to generate interrupt every 20ms, but interrupt is not fired.
I'm finding a official examples to use HAL to config TIM as internal interupt.
Any idea? any ink?
Thanks
Jordi
2018-12-14 3:48 AM
> interrupt is not fired.
Read out and check the content of relevant TIM and NVIC registers. Check in disasm that the ISR's address is correctly in the vector table.
JW
2018-12-14 6:08 AM
The TIM are all much the same, TIM1/TIM8 are typically more complex (advanced), but the others should be readily portable, basically cut-and-paste search-and-replace.
Be attentive to IRQ Handlers in the stm32f3xx_it.c file, the exact naming, callback, and NVIC, etc
2018-12-17 1:23 AM
Dear all,
thanks for you feedback.
But my problem is using HAL.
At end I got to work well, but not with all timers.
Do you know where I can found examples over HAL and CubeMX?
Thanks
Jordi