cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8T6 Program not working and USB not recognized

JTAPIE
Associate II

Hello,

I found this schematic and layout with a stm32f103c8t6. I ordered it and wanted to programm it.

With stm32cubeprogrammer I detect the stm32 no problem via ST-LINK.

Same with stm32cubeide I can download successfully the code.

But now the problem is that eventhough the code is downloaded successfully the simple program to blink a pin to which I attach a diode is not working and I don’t see why.

I also want to be able to send data from my computer to the STM32 with USB but after downloading the code with "usb_device.h" and MX_USB_DEVICE_Init();, deconnecting ST-LINK and connecting with USB the STM32 is not recognized by the computer.

Any idea of what I could look for or ressources ?

If you see any problem in the design please tell me.

Regards,

Jean

Basic_STM32_Bluepill.png

pcb.PNG

  

stm32cubeprog.PNG

code.PNG

 

download.PNG

  

17 REPLIES 17

So have you used the debugger?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

Did you get your own board working?

https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32f103c8t6-no-usb-detection/td-p/739695 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Unfortunately, our logo on an MCU does not prove at all that it is an original. STM32F103C8T6 in particular have been counterfeited on a large scale for several years, including the logo.

In cases where you cannot be completely sure that the seller is selling original goods (Aliexress, Ebay, etc.), it is advisable to check this with a test programme. You can also find tips on this here in the community, e.g. here or there.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The MCU that the manufacturer used looks like this one from the link you send, is this the one you said is counterfeit?

JTAPIE_0-1738080082112.png

 

No that's why I tried to do this new PCB.

Yes

 

 

 

Waiting for debugger connection... Debugger connected Waiting for debugger connection... Debugger connected Waiting for debugger connection... ------------------------------------------------------------------- STM32CubeProgrammer v2.15.0 ------------------------------------------------------------------- Log output file: C:\Users\JEAN~1.TAP\AppData\Local\Temp\STM32CubeProgrammer_a43840.log ST-LINK SN : E1007200D0D2139393740544 ST-LINK FW : V2J43S7 Board : -- Voltage : 3.25V SWD freq : 4000 KHz Connect mode: Under Reset Reset mode : Hardware reset Device ID : 0x410 Revision ID : Rev X Device name : STM32F101/F102/F103 Medium-density Flash size : 64 KBytes Device type : MCU Device CPU : Cortex-M3 BL Version : -- Memory Programming ... Opening and parsing file: ST-LINK_GDB_server_a43840.srec File : ST-LINK_GDB_server_a43840.srec Size : 29.80 KB Address : 0x08000000 Erasing memory corresponding to segment 0: Erasing internal memory sectors [0 29] Download in Progress: File download complete Time elapsed during download operation: 00:00:01.890 Verifying ... Download verified successfully Shutting down... Exit.
View more

 

That just shows the programmer connecting to the chip, and programming it.

Have you used the CubeIDE debugger to see what your code is actually doing?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

As I already mentioned: as long as you can't trace the supply chain in detail, nobody can say for sure, only one of the tests mentioned can clarify this.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.