‎2023-02-22 10:02 PM
I have been trying to get a TMC2209 and STM32F103 working over UART for a while now.
I have followed 2 posts ( I am pretty sure correctly ) on this but I can't add them here as I am a new member, they are already on this community.
I have found online that I need to bridge a connection at the back of the driver board I am using, I have done that.
I have also found that for the start UART comms I need to set "GCONF.pdn_disable = 1"
I think that is done correctly in the code below but feel free to correct me.
I have connected a 1K resistor between the Tx and Rx lines as in the datasheet and in one of the posts above.
My problems start with the UART connection I believe.
I have included nothing else in this code so I can just look at getting this working.
I get a 0x05 on Recv[0] each time I run the code but I do not get any other values, I expect to see 0xFF in Recv[1] but I get 0x00.
I get the sync nibble but then nothing else, when I disconnect the Rx and Tx line from the TMC2209 I still get the 0x05 so that makes me thing something is wrong there.
I have tried to use the Receive to idel but I get the same results as the above.
I have played with delays before Receving but then I don't even get the 0x05.
I worried that I might be sending the data in the wrong order ?
All I am trying to do is read back the register I just wrote to.
:
Any pointers would be great on where to go to from here.
Thanks all.
‎2023-02-22 10:03 PM
For some reason my code did not get added, here it is :
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim5;
UART_HandleTypeDef huart3;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_TIM5_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_TIM5_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
// basic testing for the TMC2209 driver, sending data on the UART line.
uint8_t send [8]; // total to send
send[0] = 0x05; // Sysnc part to start Tx
send[1] = 0x00; // Slave Addr ( to address the different drivers
send[2] = 0x80; // Addr of the register +
send[3] = 0x00;
send[4] = 0x00;
send[5] = 0x03;
send[6] = 0x2E;
send[7] = 0xEF;
HAL_UART_Transmit(&huart3, send, sizeof(send),10);
// ask for a read now from 0x02 ( IFCNT )
uint8_t Recv[8] = {0};
uint8_t send2 [4]; // total to send
send2[0] = 0x05; // Sysnc part to start Tx
send2[1] = 0x00; // Slave Addr ( to address the different drivers
send2[2] = 0x00; // Addr of the register +
send2[3] = 0x48;
HAL_UART_Transmit(&huart3, send2, sizeof(send),10);
HAL_UART_Receive(&huart3, Recv, 8, 100);
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL16;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief TIM5 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM5_Init(void)
{
/* USER CODE BEGIN TIM5_Init 0 */
/* USER CODE END TIM5_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM5_Init 1 */
/* USER CODE END TIM5_Init 1 */
htim5.Instance = TIM5;
htim5.Init.Prescaler = 50;
htim5.Init.CounterMode = TIM_COUNTERMODE_UP;
htim5.Init.Period = 100;
htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim5.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim5) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim5, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim5, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM5_Init 2 */
/* USER CODE END TIM5_Init 2 */
}
/**
* @brief USART3 Initialization Function
* @param None
* @retval None
*/
static void MX_USART3_UART_Init(void)
{
/* USER CODE BEGIN USART3_Init 0 */
/* USER CODE END USART3_Init 0 */
/* USER CODE BEGIN USART3_Init 1 */
/* USER CODE END USART3_Init 1 */
huart3.Instance = USART3;
huart3.Init.BaudRate = 115200;
huart3.Init.WordLength = UART_WORDLENGTH_8B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = UART_PARITY_NONE;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART3_Init 2 */
/* USER CODE END USART3_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
‎2023-02-23 1:02 AM
Dear @TDuck.1​
Just some ideas to check :
Is there an echo or a loop between your TX and RX pins ? In other words, could it be that when you "get a 0x05 on Recv[0]", this 0x05 is the one you sent from send[0] or send2[0] ?
Second question (if answer to first one is no) : is return code of your HAL_UART_Receive() call equal to HAL_OK ? in such case, it means you receive properly 8 bytes, right ?
Regards
‎2023-02-23 4:30 PM
Hi, so I might have an echo as you pointed out, when I try and receive after the frist Tx I still get the 0x05 but that should not happen as Write commands should not reply to anything ( from what I understand in the datasheet )
When I disconnect the Tx and Rx lines from everything then I do not get the 0x05, but when I connect them together with only the 1K resistor but not to the TMC2209 then I get a the 0x05 sync nibble.
Any suggestions on how I would get ride of that ?
I also edited the code to look if the Receive would return HAL_OK but it does not so it is not actually getting anything from the TMC2209.
Thanks for the input.
‎2023-02-23 5:35 PM
The line 126 of your code has a bug.
If you connect the Rx line to the Tx line, isn't it obvious that it receives the transmitted data? ;) One has to either ignore/clear that data or better switch from Tx to Rx mode and back. Probably the HAL_HalfDuplex_EnableTransmitter()/HAL_HalfDuplex_EnableReceiver() functions can help, if you want to stick with the HAL/Cube broken bloatware.
‎2023-02-23 8:46 PM
@Piranha​ Thanks for pointing out that bug.
I have seen that the USART line gets pulled down to around 1V when I connect it to the TMC2209, this seems like it could be a problem. I used a different board and found the mod that I did to the back was the cause of this pull down error, but now I am getting a much higher value signal but still nothing coming back from the TMC2209.
Seems like the guide I saw was incorrect about bridging the 2 pads to get UART working.
I have tried with the HAL_HalfDuplex_EnableTransmitter()/HAL_HalfDuplex_EnableReceiver() functions you suggested but using them and the UART port in Half Duplex mode returns nothing, not even that echo off the Tx line.
That and I see in your last posts that the Pin out settings do not really allow this connection :
"Therefore the 1k series resistor is mandatory and the correct pin configuration is: alternate function, push-pull, low speed, pull-up. And this configuration doesn't need to be changed at runtime."
I have set USART3 to Asynchronous mode but now I am unsure if I am sending the correct values for the Register or in the correct order, if you have any input on that I would greatly appreciate it.
‎2023-02-23 8:51 PM
Well looking at the Datasheet of my board I actually do need to bridge that pad at the back to get UART connected, but it seems werid that there is such a strong pull down on that line ?
Enough to pull it to 1V from 3.3V
‎2023-03-05 3:21 PM
Seems that by default the board is configured for standalone operation. For UART operation I would remove the R1 20k. Internal pull-up/down on STM32 is ~40k, so 1V makes sense.
Also I checked the CRC for your test examples - those are OK.
‎2024-02-11 5:31 AM
I was also struggling with the UART communication with TMC2209, in my case transmit was always working fine but receive wasn't. I solved my issue by enabling halfduplex transmitter (HAL_HalfDuplex_EnableTransmitter) before sending and enabling halfduplex receiver (HAL_HalfDuplex_EnableReceiver) before receiving. An example driver code is available on my github page (https://github.com/veysiadn/tmc_2209), the other parts of the code is modified from TMC2209 arduino library (https://github.com/janelia-arduino/TMC2209).
Good luck,
Veysi