Hi @Marosh In my understanding, you could have your definition of SNK PDOs covering various voltages and power. At the end, whatever those PDOs, decision about which SRC PDO to choose to build the REQUEST message is a SNK decision.Entry point of this...
Yes, should be better.If I understand properly your goal, you need to adjust only the "power" related fields of your SNK PDO.Please also note that some elements shown in the snapshots of PDO structures I attached in my previous post, are only provide...
Hi @Marosh SRC and SNK PDO are not built on same structure, so you cannot copy Received PDO from the SRC, into the SNK PDO of your equipement. Please check chapters 6.4.1.2 and 6.4.1.3 of Universal Serial BusPower Delivery Specification.Example for F...
I confirm @Pavel A. statement. This function aims to check TEACK/REACK status in order to conclude initialisation is properly done. No link with Idle line detection on RX.I acknowledge that function name might not be the most appropriate one.Regards
Hello @Rise Following decoding of the message header values you provided, SRC capabilities message decoding is indeed showing use of MsgID value = 1, and GoodCRC reply is shown using 7 which is not expected indeed.However, as MsgID of SRC capabiliti...