2016-12-12 3:00 AM
hi
in this doc en.DM00210526.pdf there is no name of STM32F030K6T6 to know which pin is which Chanel of touch.
and in STM32F030K6T6.pdf there is no name of touch in pin configuration.
can i use touch library on this MCU?
#touch-sense #stm32f030k6t62016-12-12 3:18 AM
Hello,
There is no touch sensing controller TSC on the STM32F030xxx.
If you need the function, use the STM32F031xxx (no usb) or the STM32F032xxx (with USB).
see the table
Best regards,
Max
2016-12-12 4:24 AM
thanks.
can i use software solution?
if its yes where can i find touch library to use in software?
2016-12-12 4:38 AM
have a look at thispost:
2016-12-13 7:25 AM
Hi
navidrct@gmail.com
I have moved this post to the
where product related questions are posted.Thanks
Oli