2016-12-24 6:15 AM
I use STM32CubeMX v4.0. It generates MX_Device.h file for configuring CMSIS-Drivers. I found that there are some macroses use hyphen symbol, which is not allowed:
/*-------------------------------- SYS --------------------------------*/
#define MX_SYS 1
/* GPIO Configuration */
/* Pin PE2 */
#define MX_SYS_TRACECLK_Pin PE2
#define MX_TRACECLK SYS_TRACECLK
/* Pin PA13 */
#define MX_SYS_JTMS-SWDIO_Pin PA13
#define MX_SWDIO SYS_JTMS-SWDIO
/* Pin PE3 */
#define MX_SYS_TRACED0_Pin PE3
#define MX_TRACED0 SYS_TRACED0
/* Pin PA14 */
#define MX_SYS_JTCK-SWCLK_Pin PA14
#define MX_SWCLK SYS_JTCK-SWCLK
/* Pin PE6 */
#define MX_SYS_TRACED3_Pin PE6
#define MX_TRACED3 SYS_TRACED3
/* Pin PE4 */
#define MX_SYS_TRACED1_Pin PE4
#define MX_TRACED1 SYS_TRACED1
/* Pin PE5 */
#define MX_SYS_TRACED2_Pin PE5
#define MX_TRACED2 SYS_TRACED2�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Solved! Go to Solution.
2017-09-13 3:55 AM
Hello
,Great thanks for your inputs.
I am able to reproduce it at my end.
The point is that MX_Device.h is generated by Cube, based on a ftl template coming from ARM.
You can find it in the F4 package, downloaded from ARM, here:
C:\Keil_v5\ARM\PACK\Keil\STM32F4xx_DFP\2.0\MDK\CubeMX
Waiting for ARM correction, you can replace the MX_Device_h.ftl template by the one I upload.
Thus, we are submitting a ticket to ARM.
Hope it help you
Kind regards
Sirma
________________ Attachments : MX_Device_h.ftl.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyS0&d=%2Fa%2F0X0000000b7n%2F6sgeMKvFhVLLcheml9DYPVOMO1SYMLEiz071VjoOBAo&asPdf=false2016-12-24 7:01 AM
Hi Eugene,
I've passed your note to the CubeMX team.
Thanks!
2017-04-09 3:24 AM
Hi
marsanne.sebastien
,Do you have any plans to fix the bug?
The bug still exists in v 4.1
2017-09-12 11:18 AM
Hello
Yauhen.Sinkevich
;Could you please let me know on which family you have observed this error ?
Great thanks in advance.
Kind regards
Sirma
2017-09-12 11:21 AM
Hello
SIRY.Marc
,It is STM32F4
Best regards,
Eugene.
2017-09-13 3:55 AM
Hello
,Great thanks for your inputs.
I am able to reproduce it at my end.
The point is that MX_Device.h is generated by Cube, based on a ftl template coming from ARM.
You can find it in the F4 package, downloaded from ARM, here:
C:\Keil_v5\ARM\PACK\Keil\STM32F4xx_DFP\2.0\MDK\CubeMX
Waiting for ARM correction, you can replace the MX_Device_h.ftl template by the one I upload.
Thus, we are submitting a ticket to ARM.
Hope it help you
Kind regards
Sirma
________________ Attachments : MX_Device_h.ftl.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyS0&d=%2Fa%2F0X0000000b7n%2F6sgeMKvFhVLLcheml9DYPVOMO1SYMLEiz071VjoOBAo&asPdf=false2017-09-13 4:06 AM
Thanks,
SIRY.Marc
, for the bug fix!