2015-03-27 01:16 AM
not working correctly setup window LTDC after opening already saved project
(see. screenshot)after generating the project is not the correct parameters are passed to the C-project:(2015-03-30 03:37 AM
not working correctly setup window LTDC after opening already saved project
Do you mean that project was generated initially with correct parameters then they were wrongly updated next time when project re-generated?Could you please share an .ioc file?Which CubeMX version are you using (last one is 4.7.0)-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-03-31 12:26 AM
project for version 4.6
However, 4.7 is identical Yes, the project had an initial generation parameters for LTDC default, after modifying the parameters are all displayed correctly and C-project also receives the correct settings LTDC. Project is saved. As described above, after the re-opening of the project there are problems ... :( ________________ Attachments : Open429.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzRI&d=%2Fa%2F0X0000000bLw%2FpvU9xLFxPeW9ZmwY_P.bmu87rTx1weECOVUE9yHZIB8&asPdf=false