cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX and LTDC configurator

Davydenko.Sergey
Associate II
Posted on March 27, 2015 at 09:16

not working correctly setup window LTDC after opening already saved project

(see. screenshot)

after generating the project is not the correct parameters are passed to the C-project

:(

  0690X00000603RxQAI.jpg

2 REPLIES 2
Amel NASRI
ST Employee
Posted on March 30, 2015 at 12:37

not working correctly setup window LTDC after opening already saved project

 

Do you mean that project was generated initially with correct parameters then they were wrongly updated next time when project re-generated?

Could you please share an .ioc file?

Which CubeMX version are you using (last one is 4.7.0)

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Davydenko.Sergey
Associate II
Posted on March 31, 2015 at 09:26

project for version 4.6

However, 4.7 is identical

Yes, the project had an initial generation parameters for LTDC default, after modifying the parameters are all displayed correctly and C-project also receives the correct settings LTDC.

Project is saved.

As described above, after the re-opening of the project there are problems ...

:(

________________

Attachments :

Open429.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzRI&d=%2Fa%2F0X0000000bLw%2FpvU9xLFxPeW9ZmwY_P.bmu87rTx1weECOVUE9yHZIB8&asPdf=false