2018-08-08 03:55 AM
Hello,
Where I can find a list of change with this version about HAL_CAN. The compatibility has been broken but there is an exhaustive list of modification?
Thanks
Bertrand
2018-08-08 02:22 PM
Seem to recall seeing a post the other week breaking down the new CAN model and differences.
2018-08-09 02:04 AM
Hello @Bertrand ,
Please find below the main changes noted in the release note for the new HAL CAN driver:
CAN driver API's compatibility is broken:
It would helpful to use a diff between the two versions to see the main changes.
Hope this helps you.
With Regards,
Imen
2018-08-09 02:35 AM
Thanks for your reply :
To Clive : Not enough familiar with this new forum to find any question about it. I will make more effort next time ;)
To ST : I have obviously read the release note but it is a bit weak to understand whats means "limitations of CAN FIFO...". In the same time, the data structure has change...
At the end, I spent time to use this version ( because of a bug of CubeMX where it is difficult ( or not possible!?) to revert to a previous FW version. I am wondernig if I have not forget to implement something with this new version even it seems to work up to now.