STM32 USART with unknown data length from the computer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-01 12:21 AM
Hello,
I am receiving UART data from the computer using my STM32 MCU with dynamic length. Sometimes the computer send 6 bytes and some time 10 bytes etc...and there is no rule for this.
Can anyone help me how to use the HAL_UART_Receive_IT in this case? Or I have to use the HAL_UART_Receive and wait for the timeout?
Thank you very much
#stm32-uart #stm32- Labels:
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-01 5:30 AM
This discussion may help you:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-01 5:46 AM
The USART itself interrupts on each character reception, you can manage things in the IRQHandler, or call into the HAL and let it call you back when it has accumulated the specified number of characters.
You are not compelled to use the HAL defined methods, if your problem can be solved with a simple ring-buffer implementation then do that. I've posted GPS examples where a line of data is accumulated in the IRQHandler and then the whole line is passed off for processing.
>>..and there is no rule for this.
But there is presumably some method or structure to the data received, if not how else can you parse it. If the data is totally lacking form do you separate groups of data by the gaps between them?
If it is a protocol you have defined you might want to refine it, or pass length details.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-01 6:36 AM
using a circular RxDMA buffer
initialize before while(1)
U1RxBufferPtrOUT = 0;
HAL_UART_Receive_DMA(&huart1, (uint8_t *)Usart1RxDMABuffer, U1RxBufSize);
you can Peek at the buffer level ;
U1RxBufferPtrIN this is pointing to the next Rx byte position.
char readableU1(void) { // returns length in DMA not read.
U1RxBufferPtrIN = U1RxBufSize - huart1.hdmarx->Instance->CNDTR; return U1RxBufferPtrIN - U1RxBufferPtrOUT;}if you want to read some bytes you use U1RxBufferPtrOUT. As you read bytes from the buffer, you must increment your U1RxBufferPtrOUT and wrap it at the DMA circular buffer length.
ie
The correct method to check the current receive buffer length is
RxLength = readableU1() // reads zero after initialization
just after initialization;
if you receive 10 bytes
U1RxBufferPtrIN = 10
and since U1RxBufferPtrOUT is still zero. : RxLength becomes 10.
You can poll this value readableU1() for your required packet size without reading a byte.
as you read each byte from that packet, you increment U1RxBufferPtrOUT and wrap at U1RxBufSize
char readU1(void) {
char readByte = Usart1RxDMABuffer[U1RxBufferPtrOUT++]; if (U1RxBufferPtrOUT >= U1RxBufSize) U1RxBufferPtrOUT = 0; return readByte;}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-01 8:30 AM
Thank you so much for your reply,
Actually I am using modbus and my MCU is a slave in an inverter which is controlled by another MCU so I can't patch guess exactly the data length from the master.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-01 8:31 AM
Thank you very much. I am following the instruction
:)