Skip to main content
SteveM732
Associate
April 10, 2025
Question

Linker script reporting incorrect SRAM size

  • April 10, 2025
  • 5 replies
  • 743 views

The linker scripts generated by MX for the STM32U5G9xx devices are reporting 2528 Kbytes of RAM. These are 3MB devices so I would expect there to be 3008 Kbytes of RAM when ECC is disabled.

 

MX output to STM32U5g9xx_FLASH.ld:

/*
** Abstract : Linker script for STM32U5G9xJ Device from STM32U5 series
** 4096Kbytes FLASH
** 2528Kbytes RAM
*/



/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 2496K
SRAM4 (xrw) : ORIGIN = 0x28000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 4096K
}

 

See Table 2 and page 27 of https://www.st.com/resource/en/datasheet/stm32u5g9vj.pdf

 

On a somewhat related note, MX in Linux wasn't generating the linker scripts so I had to use a Windows computer to generate them.

 

This topic has been closed for replies.

5 replies

STTwo-32
ST Technical Moderator
April 11, 2025

Hello @SteveM732 

Are you using the last version of the STM32CubeMX (V6.14.0). If so, could you please add a .ioc file that reproduce the same behavior (based on the STM32CubeMX V6.14.0). I'm not able to reproduce it on my side:

STTwo32_0-1744380346796.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SteveM732
SteveM732Author
Associate
April 11, 2025

Yes, it is 6.14.0.

STTwo-32
ST Technical Moderator
April 11, 2025

Hello @SteveM732 

I've opened a project based on your .ioc file on the STM32CubeIDE V1.18.0 and I've been able to find the correct RAM value. Could you send me a screenshot of the error with the last CubeIDE and MX versions.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.