2024-09-23 12:27 AM
Hello everyone,
I sent the data by UART with command:
uint16_t Size[8];
HAL_UART_Transmit_IT(UART_HandleTypeDef *huart, const uint8_t *pData, uint16_t Size)
Question: Size on this command is 16 bytes or Size is 8 data elements of array?
Solved! Go to Solution.
2024-09-23 6:16 AM
@Andrew Neil wrote:The setting is based on the current configuration of the UART
It's tested at runtime:
/* In case of 9bits/No Parity transfer, pData needs to be handled as a uint16_t pointer */
if ((huart->Init.WordLength == UART_WORDLENGTH_9B) && (huart->Init.Parity == UART_PARITY_NONE))
{
pdata8bits = NULL;
pdata16bits = (const uint16_t *) pData;
}
else
{
pdata8bits = pData;
pdata16bits = NULL;
}
this is where it makes the decision to treat the buffer as 8 or 16 bits.
@Andrew Neil wrote:
whether it is sending 9-bit data frames, or 8-bit data frames.
Clearly, you can't fill a 9-bit data frame from a single 8-bit buffer entry - you need something at least 9 bits.
C doesn't provide a 9-bit datatype - the next available option after 8 bits (single byte) is 16 bits (two bytes).
2024-09-23 12:32 AM - edited 2024-09-23 12:35 AM
See the documentation:
/**
* @brief Send an amount of data in interrupt mode.
* @note When UART parity is not enabled (PCE = 0), and Word Length is configured to 9 bits (M1-M0 = 01),
* the sent data is handled as a set of u16. In this case, Size must indicate the number
* of u16 provided through pData.
* @note When UART parity is not enabled (PCE = 0), and Word Length is configured to 9 bits (M1-M0 = 01),
* address of user data buffer containing data to be sent, should be aligned on a half word frontier (16 bits)
* (as sent data will be handled using u16 pointer cast). Depending on compilation chain,
* use of specific alignment compilation directives or pragmas might be required
* to ensure proper alignment for pData.
* huart UART handle.
* pData Pointer to data buffer (u8 or u16 data elements).
* Size Amount of data elements (u8 or u16) to be sent.
* @retval HAL status
*/
HAL_StatusTypeDef HAL_UART_Transmit_IT(UART_HandleTypeDef *huart, const uint8_t *pData, uint16_t Size)
See also the User Manual for the HAL; eg,
2024-09-23 12:36 AM - edited 2024-09-23 12:45 AM
I read this but I fill data elements, the received data is lost
I fill the byte, I received all data
So this document is not clearly, Size must be 2*data element arry (u16) or 4*data element arry (u32), right?
2024-09-23 12:53 AM - edited 2024-09-23 12:54 AM
As it says, you use u16 when the UART frame's data payload size is larger than 8 bits - therefore can't be filled using a single u8 item.
So, if you are receiving complete data byte-by-byte, that means your data must fit in 8 bit payloads - so you should not be using a u16 buffer.
Show a minimal but complete complete example which illustrates your issue.
PS:
See also the device Reference Manual - see how the parity and extra data payload bits are handled...
2024-09-23 1:01 AM
My example:
uint16_t tx_data[7];
HAL_UART_Transmit_IT(&huart1, tx_data, 7);
or
HAL_UART_Transmit_IT(&huart1, tx_data, 14);
Which transmit command is correct?
2024-09-23 1:05 AM - edited 2024-09-23 1:12 AM
that's not a complete example - is it?
@ManhPham wrote:Which transmit command is correct?
As the documentation says, It depends on how you UART is configured - 8-bit (or smaller) data, or 9-bit data.
For 9-bit data, you need two buffer bytes for each transmitted UART Frame:
|<-------------------------------------u16------------------------------------->|
+---------------------------------------+---------------------------------------+
Buffer: | -- : -- : -- : -- : -- : -- : -- : b8 | b7 : b6 : b5 : b4 : b3 : b2 : b1 : b0 |
+---------------------------------------+---------------------------------------+
PS - disclaimer: I don't know if that's the right bit/byte ordering - but you see how it takes two buffer bytes to contain the 9-bit payload?
PPS:
It's exactly the same when you use the non-interrupt method:
/**
* @brief Send an amount of data in blocking mode.
* @note When UART parity is not enabled (PCE = 0), and Word Length is configured to 9 bits (M1-M0 = 01),
* the sent data is handled as a set of u16. In this case, Size must indicate the number
* of u16 provided through pData.
* @note When UART parity is not enabled (PCE = 0), and Word Length is configured to 9 bits (M1-M0 = 01),
* address of user data buffer containing data to be sent, should be aligned on a half word frontier (16 bits)
* (as sent data will be handled using u16 pointer cast). Depending on compilation chain,
* use of specific alignment compilation directives or pragmas might be required
* to ensure proper alignment for pData.
* @PAram huart UART handle.
* @PAram pData Pointer to data buffer (u8 or u16 data elements).
* @PAram Size Amount of data elements (u8 or u16) to be sent.
* @PAram Timeout Timeout duration.
* @retval HAL status
*/
2024-09-23 1:15 AM - edited 2024-09-23 1:23 AM
2024-09-23 4:57 AM
By default it is uint8_t which is transmitted via uart. If you want to send integers, convert them to uint8_t and send . in the receiving side you have to take care to assemble it again. Does it answer your question?
2024-09-23 4:59 AM
@Techn wrote:By default it is uint8_t ?
No.
The setting is based on the current configuration of the UART - whether it is sending 9-bit data frames, or 8-bit data frames.
2024-09-23 6:16 AM
@Andrew Neil wrote:The setting is based on the current configuration of the UART
It's tested at runtime:
/* In case of 9bits/No Parity transfer, pData needs to be handled as a uint16_t pointer */
if ((huart->Init.WordLength == UART_WORDLENGTH_9B) && (huart->Init.Parity == UART_PARITY_NONE))
{
pdata8bits = NULL;
pdata16bits = (const uint16_t *) pData;
}
else
{
pdata8bits = pData;
pdata16bits = NULL;
}
this is where it makes the decision to treat the buffer as 8 or 16 bits.
@Andrew Neil wrote:
whether it is sending 9-bit data frames, or 8-bit data frames.
Clearly, you can't fill a 9-bit data frame from a single 8-bit buffer entry - you need something at least 9 bits.
C doesn't provide a 9-bit datatype - the next available option after 8 bits (single byte) is 16 bits (two bytes).