cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 truestudio gdbserver connection failed

elagreca1970
Associate II
Posted on August 22, 2015 at 17:05

Truestudio v5.3.0

stm32f407

running gdbserver in persistent mode get failed connection when trying to connect from within truestudio ide. Have to disconnect stlink power off/on target board a number of times before connection established. Was working ok for a while until now. When using stm32f103 in another project never have this problem. Has anyone experienced this very frustrating!!
2 REPLIES 2
Posted on August 24, 2015 at 17:03

Hi la_greca.emilio,

Try to run an example of the package STM32Cube_FW_F4_V1.7.0 on TrueStudio. May be the problem results from your configuration.

-Shahrzad- 

elagreca1970
Associate II
Posted on August 29, 2015 at 01:53

Problem is with USB on laptop.  Tried another laptop with same configuration, STlink and target with no problems!